STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

stm32ide project file organization

I am confused where my source file should be stored.  It seems that I have duplicate files stored in multiple locations. Some seem to get updated together and some don't!For instance I have a main.h file stored here-> FJB_KEYPAD_R5\STM32CubeIDE\Appli...

FJB2069_0-1735405320747.png
FJB2069 by Senior
  • 2602 Views
  • 4 replies
  • 2 kudos

NucleoH7S3L8 SPI Not Working

Dear ST Community,I have the following issue:I try to start a simple SPI Transmit but it seems that after a first burt of clocks which I observe on the osciloscope, the program gets stack in the Error_Handler, while it shouldn't based on .ioc configu...

DG91 by Associate
  • 1288 Views
  • 2 replies
  • 0 kudos

Resolved! Snprintf float and double issue

Hey,I am using one of the custom board for stm32f407vetx. When i was using stm32f407 disc board. There was no problem but now i cannot fill up array with float or double values. And yes i increase min heap size to 0x1000 and max heap size to 0x2000. ...

SabTuna by Associate II
  • 1308 Views
  • 1 replies
  • 0 kudos

Resolved! BLE_Beacon_AoA_Tag and Locator examples missing files

With CubeIDE Version 1.17 two examples for BLE Beacon AoA where deployed (Tag and Scanner). But I'm having trouble compiling both. After loading both examples from the STM32 Project Example Selector and building both projects I'm getting the error th...

jpepv by Associate II
  • 2043 Views
  • 4 replies
  • 0 kudos

All themes except classic break IDE tabs and icons

Windows 11 / IDE Version: 1.17.0 / Build: 23558_20241125_2245 (UTC)I tried changing the IDE's theme from classic to Dark, Light, and even Eclipse Marketplace themes. I always get some weird visuals. If I have one tab selected and hover over another, ...

Ziimag by Associate
  • 1617 Views
  • 1 replies
  • 0 kudos

Bare Metal ADC on NUCLEO-H745ZI-Q

Hello,I am troubleshooting a similar problem as described in this post TM32H7 ADC Baremetal - Cannot get ADC module readyI am using PF10 on ADC3 as it is already routed to the CN10 header. Intentionally ignoring CMSIS header/defines in the spirit of ...

Screenshot from 2024-11-26 18-02-05.png

STM32CubeIDE crashes after 2 minutes

Hello everyone!I installed STM32CubeIDE and every time when I want to start it, it crashes after two minutes. I found one solution related to the workspace here in ST community, but it doesn't work for me. Last few days I am trying to solve this prob...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.