2024-09-04 9:26 AM - edited 2024-09-04 9:31 AM
Hello, after I upgraded my ubuntu STM32CubeIDE from 1.14.0 to 1.16.0 I am getting the IDE menus messed up, menu fonts messed up and some portions of the screen are black. Previous version 1.14.0 (and respective toolchain) did not have any problem.
My laptop is System76 with Ubuntu 22.04.4.LTS , Window system Wayland, Gnome v. 42.9, all packages are the latest. All the latest Ubuntu packages were updated and I still used IDE v. 1.14.0 - everything was fine. Only after the IDE upgrade to 1.16.0 (nothing else was changed in the system) the screen got messed up. After yet a repeated re-installation (1st delete all previously installed versions of IDE, then re-install) of V. 1.16.0 IDE looked fine but after the laptop was suspended and woke up, the same problem with screen repeated. My working preferences were imported - didn't help. I switched the IDE theme setting to another theme style in order to update the IDE windows , restarted - didn't help. Screenshot is attached.
Please help - our project stuck.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.