2026-01-06 9:44 AM
I have a working project in STM32CubeIDE v1.19 for my STM32WB55RG board. Pretty simple as it reads some sensor data, does an FFT and sends a couple results over Bluetooth. It is working well and I'm happy with the performance. I am on macos Tahoe and the highlighting of text in the editor is not working so I thought I'd upgrade to v2.0 to try to fix that problem.....what could possibly go wrong right?
STM32CubeIDE v2.0 and standalone STM32CubeMX v6.16.1 install fine and I import the project into a new workspace and if I compile immediately after importing, it compiles fine....no errors. I open the existing .ioc file in CubeMX and everything seems to load fine. I make no changes and hit "Generate Code" just to make sure the new workflow is working properly. No changes made but it apparently overwrites the existing app_ble.c file as a compile after refreshing the work done by CubeMX yields the following errors (snippets of output shown for brevity):
../STM32_WPAN/App/app_ble.c: In function 'SVCCTL_App_Notification':
../STM32_WPAN/App/app_ble.c:668:14: error: 'ACI_HAL_WARNING_VSEVT_CODE' undeclared (first use in this function); did you mean 'ACI_HAL_FW_ERROR_VSEVT_CODE'?
../STM32_WPAN/App/app_ble.c:670:11: error: unknown type name 'aci_hal_warning_event_rp0'; did you mean 'aci_hal_fw_error_event_rp0'?
arm-none-eabi-gcc "../Middlewares/ST/STM32_WPAN/ble/svc/Src/svc_ctl.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DARM_FAST_ALLOW_TABLES -DARM_ALL_FAST_TABLES -DARM_ALL_FFT_TABLES -DARM_FFT_ALLOW_TABLES -DARM_MATH_CM4 -DARM_MATH_LOOPUNROLL -DUSE_HAL_DRIVER -DSTM32WB55xx -c -I../Core/Inc -I../Drivers/STM32WBxx_HAL_Driver/Inc -I../Drivers/STM32WBxx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32WBxx/Include -I../Drivers/CMSIS/Include -I../STM32_WPAN/App -I../Utilities/lpm/tiny_lpm -I../Middlewares/ST/STM32_WPAN -I../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread -I../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread/tl -I../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread/shci -I../Middlewares/ST/STM32_WPAN/utilities -I../Middlewares/ST/STM32_WPAN/ble/core -I../Middlewares/ST/STM32_WPAN/ble/core/auto -I../Middlewares/ST/STM32_WPAN/ble/core/template -I../Middlewares/ST/STM32_WPAN/ble/svc/Inc -I../Middlewares/ST/STM32_WPAN/ble/svc/Src -I../Utilities/sequencer -I../Middlewares/ST/STM32_WPAN/ble -O3 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Middlewares/ST/STM32_WPAN/ble/svc/Src/svc_ctl.d" -MT"Middlewares/ST/STM32_WPAN/ble/svc/Src/svc_ctl.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Middlewares/ST/STM32_WPAN/ble/svc/Src/svc_ctl.o"
arm-none-eabi-gcc "../Middlewares/ST/STM32_WPAN/ble/core/template/osal.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DDEBUG -DARM_FAST_ALLOW_TABLES -DARM_ALL_FAST_TABLES -DARM_ALL_FFT_TABLES -DARM_FFT_ALLOW_TABLES -DARM_MATH_CM4 -DARM_MATH_LOOPUNROLL -DUSE_HAL_DRIVER -DSTM32WB55xx -c -I../Core/Inc -I../Drivers/STM32WBxx_HAL_Driver/Inc -I../Drivers/STM32WBxx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32WBxx/Include -I../Drivers/CMSIS/Include -I../STM32_WPAN/App -I../Utilities/lpm/tiny_lpm -I../Middlewares/ST/STM32_WPAN -I../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread -I../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread/tl -I../Middlewares/ST/STM32_WPAN/interface/patterns/ble_thread/shci -I../Middlewares/ST/STM32_WPAN/utilities -I../Middlewares/ST/STM32_WPAN/ble/core -I../Middlewares/ST/STM32_WPAN/ble/core/auto -I../Middlewares/ST/STM32_WPAN/ble/core/template -I../Middlewares/ST/STM32_WPAN/ble/svc/Inc -I../Middlewares/ST/STM32_WPAN/ble/svc/Src -I../Utilities/sequencer -I../Middlewares/ST/STM32_WPAN/ble -O3 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Middlewares/ST/STM32_WPAN/ble/core/template/osal.d" -MT"Middlewares/ST/STM32_WPAN/ble/core/template/osal.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Middlewares/ST/STM32_WPAN/ble/core/template/osal.o"
../STM32_WPAN/App/app_ble.c:672:34: error: 'aci_hal_warning_event_rp0' undeclared (first use in this function); did you mean 'aci_hal_fw_error_event_rp0'?
../STM32_WPAN/App/app_ble.c:675:65: error: request for member 'Warning_Type' in something not a structure or union
675 | APP_DBG_MSG("Warning Type = 0x%02X\n", p_warning_event->Warning_Type);
../STM32_WPAN/App/app_ble.c:757:35: error: 'CONFIG_DATA_PUBLIC_ADDRESS_OFFSET' undeclared (first use in this function); did you mean 'CONFIG_DATA_RANDOM_ADDRESS_OFFSET'?
../STM32_WPAN/App/app_ble.c:757:70: error: 'CONFIG_DATA_PUBLIC_ADDRESS_LEN' undeclared (first use in this function); did you mean 'CONFIG_DATA_RANDOM_ADDRESS_LEN'?
Now the easy fix is uninstall v2.0 and go back to v1.19 but at some point I need to move on so am hoping you can help me understand why the project will no longer compile?
I'm at a loss to troubleshoot at this point so any pointers would be helpful.
Thank You
Solved! Go to Solution.
2026-01-11 7:47 AM
To close this off, I wanted to reply saying this turned out to NOT be a v2.0 versus a v.1.19 issue. The issue persists in v1.19 and allowing CubeMX to generate code causes the issue. I had to add the following code to app_ble.c to allow my project to use CubeMX, generate code, and eliminate the errors that were tripping me up earlier:
/* --- CUBEMX MIGRATION PATCH START --- */
#ifndef ACI_HAL_WARNING_VSEVT_CODE
// 1. Fix the Event Code
#define ACI_HAL_WARNING_VSEVT_CODE ACI_HAL_FW_ERROR_VSEVT_CODE
// 2. Fix the Struct Type
typedef aci_hal_fw_error_event_rp0 aci_hal_warning_event_rp0;
// 3. Fix the Struct Member Name (The Dirty Hack)
// This renames ".Warning_Type" to ".FW_Error_Type" everywhere in this file
#define Warning_Type FW_Error_Type
// 4. Fix the Public Address Constants
#define CONFIG_DATA_PUBLIC_ADDRESS_OFFSET CONFIG_DATA_PUBADDR_OFFSET
#define CONFIG_DATA_PUBLIC_ADDRESS_LEN CONFIG_DATA_PUBADDR_LEN
#endifHope this can help someone else as it stumped me for a few days.
2026-01-06 10:03 AM
Note that you can have multiple versions of CubeIDE installed and in use at the same time on the same computer - you just need a separate workspace for each.
Have you tried recreating the app from scratch in v2.0.0 ?
2026-01-06 10:57 AM
I have not tried re-creating the project from scratch in v2.0. Maybe I'm being lazy, but starting over just to recreate something I have would force me back to v1.19 first. I will try to parallel version installation as I honestly didn't know that was an option.
For reference, I have tried to compile with v1.14 firmware and v1.19 firmware specified in STM32CubeMX Project Manager but no improvements. I will continue to chip away and report anything relevant.
2026-01-11 7:47 AM
To close this off, I wanted to reply saying this turned out to NOT be a v2.0 versus a v.1.19 issue. The issue persists in v1.19 and allowing CubeMX to generate code causes the issue. I had to add the following code to app_ble.c to allow my project to use CubeMX, generate code, and eliminate the errors that were tripping me up earlier:
/* --- CUBEMX MIGRATION PATCH START --- */
#ifndef ACI_HAL_WARNING_VSEVT_CODE
// 1. Fix the Event Code
#define ACI_HAL_WARNING_VSEVT_CODE ACI_HAL_FW_ERROR_VSEVT_CODE
// 2. Fix the Struct Type
typedef aci_hal_fw_error_event_rp0 aci_hal_warning_event_rp0;
// 3. Fix the Struct Member Name (The Dirty Hack)
// This renames ".Warning_Type" to ".FW_Error_Type" everywhere in this file
#define Warning_Type FW_Error_Type
// 4. Fix the Public Address Constants
#define CONFIG_DATA_PUBLIC_ADDRESS_OFFSET CONFIG_DATA_PUBADDR_OFFSET
#define CONFIG_DATA_PUBLIC_ADDRESS_LEN CONFIG_DATA_PUBADDR_LEN
#endifHope this can help someone else as it stumped me for a few days.
2026-01-12 1:53 AM
@WP wrote:Hope this can help someone else as it stumped me for a few days.
You can help them to find it by marking the solution:
Help others to solve their issues
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.