2022-10-16 3:45 PM
I added a c source file to an existing folder in my project and it shows in the project explorer.
When I build the project or build the individual file it appears to compile (in the console). But references to functions in the file come back as undefined. Also if I introduce deliberate errors in the source file; it compiles without errors.
What could be going on?
2022-10-17 4:51 AM
I found the problem.
The editor was not properly indicating the state of an "#ifdef", i.e. it did not gray out the code even though the value was not defined.
I have come to rely heavily on this feature.
I guess the question now is:
"Why doesn't the editor gray out the code properly?"
2022-10-17 6:34 AM
Check the related Eclipse editor parameters. These parameters are reset when a new workspace is created.
2022-10-17 9:07 AM
I am not sure where to look for those parameters - but it only fails on this one new file. In all of the other files in my project the editor grays out #ifdef'ed code.
Does each source file somehow have separate editor settings?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.