STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1703 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 638 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

How to enable / configure dynamic breakpoint ?

Hey hi Community !I’m here because I didn’t found informations onto «fonction breakpoint» «event breakpoint» and «watchpoint» :I work with STM32G071, write C and use GDB.I want to configure a conditional breakpoint, that break when a variable is equa...

PSimo.4 by Associate II
  • 4494 Views
  • 4 replies
  • 0 kudos

Wrong addresses in the Memory Browser of the debug view

Inside the Memory View window in the debug view, most of the times the addresses that are displayed when hovering the mouse over a memory cell are incorrect.For example, in the screenshot below, it should be showing 0x20000000 but instead it shows 0x...

0693W000005D0z5QAC.png 0693W000005D0zFQAS.png 0693W000005D0zPQAS.png 0693W000005D10rQAC.png
kioan by Associate
  • 1486 Views
  • 1 replies
  • 0 kudos

STM32CUBEIDE and Keil

Can I use STM32CUBEIDE to fully replace KEIL?I am considering using Mac-based STM32CUBEIDE for programming. Does STM32CUBEIDE support other non-STM32 product applications? Like debugging.Thanks!

FWu.3 by Associate III
  • 1564 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeIDE 1.10.1 compiles files twice

I noticed a problem with STM32CubeIDE 1.10.1:When build, a second time, the same files as before get compiled again.All my projects were migrated from 1.9.Steps to reproduce:Modify a fileRun the build, it compiles that fileRun the build, it compiles ...

undefined reference to `HAL_DFSDM_ChannelInit'

I'm using the BSP audio functions in my application. All of this is unmodified and straight from github. My current problem is the linker being unable to find several of the HAL_DFSDM functions called from STM32F769i_discovery_audio.c. The really puz...

IWhit.2 by Associate II
  • 1405 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.