STM32CubeIDE for Visual Studio Code (MCUs)

Ask questions on the STM32CubeIDE for Visual Studio Code extension. Find answers on a variety of topics, including build issues, debug functionalities, CMake project integration, and feature requests for CubeCLT installation.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Run without debugging on VSCode

I have setup STM32 VSCode extension on my PC and it is amazing. The only problem that I have encountered is that it is not possible to run the code without debugging. I removed the "runToEntryPoint": "main" line in launch.json. But every time I launc...

DamianoF by Associate III
  • 11702 Views
  • 24 replies
  • 9 kudos

Temporary Unavailability of Server Update Pack – Maintenance on February 26

Dear Community Members,   Please be informed that the Server Update Pack will be temporarily unavailable on February 26 due to scheduled maintenance. Date: February 26Time: From 7:00 AM (for approximately 1 hour) Central European Time (CET)   During ...

Resolved! Setup as STM32Cube project fails

I'm encountering a persistent issue when setting up an STM32Cube project in VS Code. Even when reverting to a previously working commit or starting a fresh setup from scratch (using the "Setup as an STM32Cube project" button), the process fails.The f...

DamianoF by Associate III
  • 697 Views
  • 4 replies
  • 2 kudos