2025-11-27 5:15 AM - edited 2025-12-01 1:15 AM
Hello ST team,
I am facing a reproducible issue with USART6 on the STM32MP257F-DK board when working with the OpenSTLinux 6.6.78-stm32mp-r2 distribution.
When I enable USART6 in the Linux Device Tree and deploy the DTB on the target:
SSH access breaks completely after reboot
(ssh root@192.168.7.1 no longer works)
When running a simple A35 UART6 echo application via minicom,
the entire board resets.
The reset is triggered by RIFSC / SERC firewall exceptions.
The very same DTS configuration works perfectly on OpenSTLinux 6.6.48 —
no SSH issue, no kernel panic, and UART6 user application runs fine.
This strongly suggests a firewall / RIF / OP-TEE integration regression between OSTL 6.0.0 and 6.6.78.
&usart6 {
pinctrl-names = "default", "idle", "sleep";
pinctrl-0 = <&usart6_pins_a>;
pinctrl-1 = <&usart6_idle_pins_a>;
pinctrl-2 = <&usart6_sleep_pins_a>;
status = "okay";
/* even deleting DMA properties does not avoid the crash */
/delete-property/dmas;
/delete-property/dma-names;
};As soon as this node is active, the issue appears.
When executing a simple UART send/receive application on ttySTM6,
the board resets with SError and OP-TEE panic:
E/TC:0 stm32_serc_handle_ilac:133 SERC exceptions [63:32]: 0x10
E/TC:0 stm32_serc_handle_ilac:139 SERC exception ID: 36
[ 321.848663] SError Interrupt on CPU1, code 0x00000000bf000002 -- SError
[ 321.848691] Hardware name: STMicroelectronics STM32MP257F-DK Discovery Board (DT)
[ 321.848863] Kernel panic - not syncing: Asynchronous SError Interrupt
...
[ 322.122425] ---[ end Kernel panic - not syncing: Asynchronous SError Interrupt ]---
E/TC:0 Panic 'Watchdog' at stm32_iwdg.c:218 <stm32_iwdg_it_handler>
This suggests:
RIF / SERC access violation on USART6 peripheral or DMA/LLI RAM
OP-TEE halting system due to firewall violation
Issue occurs only in OpenSTLinux 6.6.78-stm32mp-r2.
No issue in OSTL 6.0.0 with the same DTS and same application.
Removing DMA for USART6 does not prevent OP-TEE SERC panic.
USART6 appears in:
Kernel DTS
OP-TEE RIF protection DTS (stm32mp257f-dk-ca35tdcid-rif.dtsi)
Suspected regression:
RIFSC default configuration for USART6 changed
CID filtering / semaphore / privilege setup may be stricter in 6.6.78
OP-TEE RIFPROT macro now requires 8 arguments instead of 5 (breaking older config)
Could ST confirm whether:
USART6 requires an explicit RIF configuration in OP-TEE in OSTL 6.6.78?
The default RIFPROT configuration for USART6 changed between 6.0.0 and 6.6.78?
There is any known issue with:
DMA3 LLI memory region
USART6 CID filtering
Missing SCID / privilege attributes in the RIF dtsi?
Any guidance on the correct OP-TEE RIF protection entry for USART6 would be appreciated.
Board: STM32MP257F-DK
OS: OpenSTLinux 6.6.78-stm32mp-r2
OP-TEE: 4.0.0-stm32mp-r2 (supplied with OSTL)
Boot: SD card
Reproduction: 100% consistent
Please advise how USART6 is meant to be configured under OSTL 6.6.x and whether any RIF updates are required in the OP-TEE DT for correct operation.
Thank you.
2025-12-01 12:25 AM - edited 2025-12-01 1:42 AM
Hello @jumman_JHINGA,
Feel free to have a look into this conversation.
BR,
Christophe
2025-12-01 1:14 AM
link is not reachable .
2025-12-01 1:43 AM
My bad : link updated.
2025-12-03 11:36 PM
I disabled the M33 firmware loading using the following commands:
systemctl stop st-m33firmware-load.service
systemctl disable st-m33firmware-load.service
tAfter that, I updated the Device Tree to include the USART6 clock configuration:
&usart6 {
pinctrl-names = "default", "idle", "sleep";
pinctrl-0 = <&usart6_pins_a>;
pinctrl-1 = <&usart6_idle_pins_a>;
pinctrl-2 = <&usart6_sleep_pins_a>;
/* uart-has-rtscts; */
clocks = <&rcc CK_KER_USART6>;
status = "okay";
};With these changes, UART6 works correctly and I no longer encounter the SERC-related kernel panic.
However, the SSH connection still drops whenever USART6 is enabled in the DTS.
Following the guidance from this ST post:
https://community.st.com/t5/stm32-mpus-embedded-software-and/stm32mp257-usart-and-serc-exception/m-p/860815#M5358
I removed the _TRACE flag from USBPD_DRP_UCSI, recompiled the firmware, and redeployed the ELF to the target. After re-enabling the M33 firmware, the behavior remains the same: SSH stays down as long as USART6 is enabled in the DTS. Disabling the USART6 node immediately restores SSH functionality.
I would appreciate further guidance on what may still be triggering this conflict between USART6 and the SSH/network subsystem.
2026-01-29 2:39 PM - edited 2026-01-29 2:49 PM
@jumman_JHINGA @Christophe Guibout
The clock
clocks = <&rcc CK_KER_USART6>;Is already defined inside the node. Look at the "stm32mp251.dtsi" file of the linux kernel.
It's werid that you need to include that line in your device tree. This must be a bug I guess...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.