2021-10-17 4:31 AM
Hey.. there
I hope all are doing well
I have just upgraded my Ubuntu desktop version from 18.0 to 20.04
Right now, I'm playing with STM32MP1 and that's how to flash the new image i have downloaded the STM32Cube programmer Linux version 2.8.0
After successfully downloading when i try to run the programmer from the search bar then it's unable to run
When i try to run from the command line then, at the same time I'm getting following JRE errors
Can any one leads me the right solution?
All suggestions and comments welcome :)
Many Thanks
./STM32CubeProgrammerLauncher
/home/mahendra/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin
chdir /home/mahendra/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/.
current dir /home/mahendra/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin
(java:10912): Gdk-CRITICAL **: 16:49:55.369: gdk_x11_display_set_window_scale: assertion 'GDK_IS_X11_DISPLAY (display)' failed
#
# A fatal error has been detected by the Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0x00007fb5cd4a9a30, pid=10912, tid=0x00007fb5bc316640
#
# JRE version: OpenJDK Runtime Environment (8.0_265-b01) (build 1.8.0_265-b01)
# Java VM: OpenJDK 64-Bit Server VM (25.265-b01 mixed mode linux-amd64 compressed oops)
# Problematic frame:
# C [libX11.so.6+0x2ba30] XInternAtom+0x40
#
# Failed to write core dump. Core dumps have been disabled. To enable core dumping, try "ulimit -c unlimited" before starting Java again
#
# An error report file with more information is saved as:
# /home/mahendra/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/hs_err_pid10912.log
#
# If you would like to submit a bug report, please visit:
# http://bugreport.java.com/bugreport/crash.jsp
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#
Aborted (core dumped)
Solved! Go to Solution.
2021-10-20 1:43 AM
Hello,
Ok I'm sorry I was not clear enough. I understand your issue, please can you use a console and go inside your folder: /home/mahendra/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin
cd /home/mahendra/STMicroelectronics/STM32Cube/STM32CubeProgrammer/binThen run the binary STM32CubeProgrammer:
./STM32CubeProgrammer &Normally the GUI appears.
Please tell me if this way doesn't work too.
Regards,
Kévin
2021-10-19 6:25 AM
Hi @Mahendra Sondagar ,
The error is not related to the Ubuntu version, but the way you launch the STM32CubeProgrammer.
You have to run STM32CubeProgrammer and not the launcher.
If you edit the file STM32CubeProgrammer, you can see that this is a script that set environment variable, then runs correctly the launcher.
In the wiki, a page explains how to run the GUI, part 1.1.1.1.2.6 Populate the SDCard of https://wiki.st.com/stm32mpu/index.php?title=Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start/Populate_the_target_and_boot_the_image
Regards,
Kévin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2021-10-20 1:20 AM
Hi.. @Kevin HUBER
Thanks for you feedback
Yes, i also followed the STM32MP1 Wiki page that you have mentioned in to above URL
At that time, after installing the programmer, when i try to open the programmer from my installed software search menu , it was not opening!
2021-10-20 1:43 AM
Hello,
Ok I'm sorry I was not clear enough. I understand your issue, please can you use a console and go inside your folder: /home/mahendra/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin
cd /home/mahendra/STMicroelectronics/STM32Cube/STM32CubeProgrammer/binThen run the binary STM32CubeProgrammer:
./STM32CubeProgrammer &Normally the GUI appears.
Please tell me if this way doesn't work too.
Regards,
Kévin
2021-10-22 4:05 AM
Hey.. @Kevin HUBER
Thanks for your feedback
I'll check it by today
Thanks
2021-10-27 5:57 AM
Thanks
The issue have been resolved :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.