2019-10-07 2:41 AM
I upgraded CubeMX (linux OS) to Version 5.3.0 and the devicetree file is not compiling anymore.
I'm attaching the ioc File and the dts for reference.
it seems some properties (automatically generated) have the string "sleep_sleep" appended which seems wrong to me - I corrected these properties (by editing the dts file) - I got it to compile successfully but the kernel doesn't start now.
This process was working fine with an older CubeMX.
Aurelian
2019-10-08 12:03 PM
Hi @Community member
Thanks to raise this issue and sorry for inconvenience.
It will require few days to analyze. I will keep you posted.
You mention Linux OS. Did you test and find a different behavior with Windows version ?
Thanks
Olivier
2019-10-08 11:05 PM
I'm using a linux machine for development (cross compliling for STM32MPxxx) - however I'm a hardware engineer. I came across this bug when I was trying to enable UART7 & USART3 with RTS/CTS - in the previous version of CubeMx I got the two serial ports working (the device tree was fine) but the flow control wasn't working so I attempted to upgrade CubeMX hoping for the best.
I would be nice to have the uarts/usarts working withor w/o flow control working.
Thanks for looking into this issue.
Aurelian
2019-10-10 6:42 AM
Hi @Community member
I failed to reproduce your issue with "sleep_sleep" concatenation in Device Tree with CubeMX5.3.
Surprisingly when I open project you have attached I have been prompt to migrate a project from CubeMX5.2.1 not CubeMX5.3.
When moving your project to 5.3 did you get prompt and did you choose "migrate" ?
For RTS/CTS topic with UART7 and USART3 we are working on it will soon give feedback on the relevant post.
Olivier
2019-10-10 6:53 AM
Just reproduce the problem by choosing to not migrate the project.
I will escalate this point internally
BR,
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.