2022-06-07 11:53 PM
Hello ST community,
For a project, we use the STM32MP157F-EV1 where we are trying to implement the secure boot chain. For this, we have to generate a FIP package that contains all required certificates.
In the ST wiki two methods are proposed :
The second method doesn't work from my side. I have a build error. Here is my modus operandi :
./opt/st/stm32mp1/3.1-openstlinux-5.10-dunfell-mp1-21-03-31/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabicd <Developer_Package_directory>/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.4.r1-r0/tf-a-stm32mp-2.4.r1make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 \ MBEDTLS_DIR=~/mbedtls \
AARCH32_SP=sp_min \
BL33=../../u-boot-stm32mp-2020.10.r1-r0/deploy/u-boot-nodtb-stm32mp15.bin BL33_CFG=../../u-boot-stm32mp-2020.10.r1-r0/deploy/u-boot-stm32mp157f-ev1-trusted.dtb \
DTB_FILE_NAME=stm32mp157f-ev1.dtb TRUSTED_BOARD_BOOT=1 GENERATE_COT=1 ROT_KEY=<private_key_path>Including bl32/sp_min/sp_min.mk LD /home/ag/STM32mp1_Ecosystem_5.10/Developer_Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.4.r1-r0/tf-a-stm32mp-2.4.r1/build/stm32mp1/release/bl32/bl32.elfarm-ostl-linux-gnueabi-ld.bfd:
unrecognized option '-Wl,-O1'arm-ostl-linux-gnueabi-ld.bfd: use the --help option for usage informationmake:
*** [Makefile:1122: /home/ag/STM32mp1_Ecosystem_5.10/Developer_Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.4.r1-r0/tf-a-stm32mp-2.4.r1/build/stm32mp1/release/bl32/bl32.elf] Error 1This output makes me think that LDFLAGS that shall be given to GCC are given to LD directly. Does anyone have an idea of why this procedure doesn't work?
Many thanks for considering my request.
Solved! Go to Solution.
2022-06-10 8:16 AM
Hi NRixh.1 (Community Member)
Yes indeed, as described here:
https://wiki.st.com/stm32mpu/wiki/How_to_configure_TF-A_BL2
unset LDFLAGS;
unset CFLAGS;
then lauch the build.
Regards,
Olivier
2022-06-10 8:16 AM
Hi NRixh.1 (Community Member)
Yes indeed, as described here:
https://wiki.st.com/stm32mpu/wiki/How_to_configure_TF-A_BL2
unset LDFLAGS;
unset CFLAGS;
then lauch the build.
Regards,
Olivier
2022-06-12 10:55 PM
Hi OlivierK,
Sorry for the disappointment. I don't know why I saw that I had to only unset LDFLAGS.
Regards,
Nicolas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.