STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 504 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Cannot boot my original board which STM32MP151CAA3 MPU is mounted on with original device tree generated by STM32CubeMX

I'm trying to boot my original board which STM32MP151CAA3 MPU is mounted on with original device tree.However, cannot boot the board when following steps.​--Environment--​ Host PC: Intel Core i7 3.6GHz / Ubuntu Ver16.04.6 LTS STM32CubeMX: Version 5.6...

HMasu.1 by Senior
  • 3273 Views
  • 7 replies
  • 0 kudos

Resolved! IAR and Engineering Mode

I have a STM32MP157c-DK2, programming on Windows-10.What works: Build Yocto, adapt it, flash the image to the SD-Card.Use STM32CubeIDE to program and debug code on CM4My goal is to setup a proper workflow of the project, where I can integrate our sta...

Led by Senior
  • 9871 Views
  • 20 replies
  • 0 kudos

ADC issue

Hi!   I am trying to use ADC on STM32MP157C-DK2.   With Starter Package image it runs fine, but with st-example-image-qt it stuck on the function below.   Can somebody helps me with this? I think it is a problem in the device tree file.   if(HAL_ADC...

lenonrt by Associate III
  • 1416 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.