2020-03-30 1:12 AM
Cannot select 8 bit wide bus for SDMMC controller (for use with e-mmc)
Cannot select USB:OTG_LS instead of USB_OTG_FS (to use 2 usb HS and the usb OTG LS togheter)
2020-03-30 2:47 AM
Hello @PMort.1 ,
Thanks for your feedback,
For the second point : it's on going.
For the first point : Could you please share your ioc file ? because the 8 bits wide bus can be selected on my side.
Regards,
Khouloud
2020-03-30 3:56 AM
Thanks for your reply
I have found the 8 bìt bus, it is only on the SDMMC2 controller; now i can select it (MMC 8 bits wide bus)
Regards
Paolo
2020-03-30 4:03 AM
So no problem for the SDMMC ?
2020-03-30 4:33 AM
Thanks
No i can choose from 1bit to 8bit for SDMMC2, without any problem.
Best regards
Paolo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.