STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 505 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32MP157A, enable USART2 through ST-LINK

Hi,   I have a STM32MP157A-EV1 board. I'm running it in the engineering boot mode and programming the Cortex-M4 directly through the STM32CubeIDE. At the moment, I do not use the Cortex-A7.   I would like to enable USART2 and use it through the ST-LI...

0693W00000VOTVUQA5.png 0693W00000VOTVjQAP.png
Fnx_QT by Associate III
  • 3304 Views
  • 4 replies
  • 0 kudos

Resolved! How to use JLink with STM32CubeIDE v1.3.0

Hi, I saw the release document of STM32CubeIDE v1.3.0 that says supported use the JLink debugger. So I try to use JLink with STM32CubeIDE v1.3.0 on my pc (the os is Debian 9 ). But I saw the console has some error. It's shows cann't detect the MPU co...

SChen.11 by Associate III
  • 9843 Views
  • 3 replies
  • 0 kudos

Managing Interrupts in M4

Hello,   I am trying to manage some interrupts in the M4, specifically the Tamper Interrupt.   Using the STM32CubeIDE (CubeMX) I am unable to select the Tamper interrupt that shows in the NVIC peripheral, when I select it, it gets deselected automati...

AGamb.4 by Associate III
  • 1745 Views
  • 1 replies
  • 0 kudos

Resolved! Install OpenSTLinux sources offline computer

Good morning,I am trying to setup STM32CubeIDE to work on an offline computer, I do not have the option to connect it to the internet. Installing the SDK through the IDE works fine and I am able to import the OpenSTLinux source projects (Linux, U-Boo...

AGamb.4 by Associate III
  • 2917 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP1- What is order of OTP Hash key?

Example I have array of bytes: 0x1, 0x2, 0x3, 0x4, 0x5, 0x6, 0x7, 0x8....when I use command STM32CubeProgram CLI command, value should be:value = 0x12345678 or:value = 0x78563412 or:value = 0x34127856I saw wiki mention about this few days ago, but co...

Dat Tran by Senior II
  • 1374 Views
  • 1 replies
  • 0 kudos

Resolved! TF-A Exception on boot-up

I have a custom board built upon the stm32mp157f. (Therefore, have custom device trees.)I currently am seeing an exception in TF-A that I cannot explain.INFO: Reset reason (0x14): INFO: Pad Reset from NRST INFO: PMIC version = 0x21 INFO: ...

user_ABCD by Associate II
  • 6557 Views
  • 15 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.