STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 505 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 392 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Redundant FIP/u-boot in stm32mp157

Hi,Our goal is to make FIP redundant. We are using RAUC mechanism to update TF-A and FIP. Manually, using `rauc install` CLI tool, I am able to update both TF-A and FIP. If I reboot the system, new TF-A and new FIP is loaded. However, when I created ...

Why STM32cubeProgrammer suddenly stopped working & OpenFile tab is not accepting mouse click, Neither navigating to brows file option?

@hello, I was using STM32Cubeprogrammer for long time but suddenly Its main function of browsing and selection file option (OpenFile) stopped working. After multiple time install and uninstall it has the same behavior in a particular PC. I tried olde...

0693W00000Un8uPQAR.png
PS.2 by Associate II
  • 6100 Views
  • 8 replies
  • 3 kudos

Resolved! System reset during kernel debug

Using MP135F-DK board.Setup the environment and rebuild kernel.After I use openocd and gdb success connect to linux system, try to debug linux kernel, then run some simple gdb command like "bt" or do nothing, then system get reset.I did not get much ...

mingming by Associate II
  • 11096 Views
  • 16 replies
  • 0 kudos

STM32MP135F-DK

Experiencing a 'Connection timed out' error (Failed to execute MI command) in STM32Cube IDE when launching. Looking for assistance with debugger configuration and troubleshooting steps. Any advice appreciated. Thanks!

Screenshot 2023-11-08 104549.png

STM32CubeIDE 1.14.0 released

STM32CubeIDE 1.14.0 was released today on st.com as well as an in-tool update patch. What is new in 1.14.0? Added the support for new microcontrollers in the STM32WB seriesAdded the support for two new boards related to the STM32WB series: NUCLEO-WBA...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.