2019-09-15 5:38 PM
Hello,
I read the related wiki page and low power mode document.
I can enter low power mode with the command "echo mem > /sys/power/state". Thats great.
My M4 program is still running in the background. I am reading a sensor in this program. If it reads above 30 Celcius or the user touches the touch screen, I want the MPU to exit low power mode.
What should I exactly do ?
With what should I play in m4 code ?
tnx
Solved! Go to Solution.
2019-09-16 12:48 AM
Hi @IYetk
You might configure the source of wakeup matching your need.
eg you can refer to Cube Package exemple "OpenAMP_TTY_echo_wakeup"
Use case "2) System Run Mode with CA7 in CStop and CM4 in CRun" you have an example to wakeup A7 from M4 message. ( might fit your >30° use case)
Guess it can also give you some clue to then set wakeup source for Touch Screen event.
Olivier
2019-09-16 12:48 AM
Hi @IYetk
You might configure the source of wakeup matching your need.
eg you can refer to Cube Package exemple "OpenAMP_TTY_echo_wakeup"
Use case "2) System Run Mode with CA7 in CStop and CM4 in CRun" you have an example to wakeup A7 from M4 message. ( might fit your >30° use case)
Guess it can also give you some clue to then set wakeup source for Touch Screen event.
Olivier
2019-09-16 4:39 AM
thank you very much
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.