2019-09-14 6:33 AM
i mean do the update somehow on the fly without removing the card from a running system, on the pc build a new rootfs and instead of removing the card, and do the copying on the pc, do this directly on the dk board. in principle it should be possible, i just need the 'magic' commands/scripts, or even have this new rootfs in ram on some ram drive
e.g. scp the new rootfs, then chroot to it, somehow
2019-09-16 2:41 AM
Hi @yakabmarci
By connecting your board with ethernet you can update rootfs via "scp",then "sync" command to write it to SD-Card.
You have also solution to use remote rootfs via nfs or tftp server.
This page can help :
https://wiki.st.com/stm32mpu/wiki/How_to_boot_the_kernel_via_TFTP_from_U-Boot
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.