STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP1 BootLin BlogPost

Dear STM32 MPU Community,Please find below some technical STM32MP1 BlogPost from our partner Bootlin :https://bootlin.com/blog/building-a-linux-system-for-the-stm32mp1-basic-system/https://bootlin.com/blog/building-a-linux-system-for-the-stm32mp1-co...

KKHOL by ST Employee
  • 1932 Views
  • 3 replies
  • 6 kudos

Resolved! PANIC during wake up MPU

Hello.I have a DK2 board and I want to wake up MPU (CA7) after shutdown command. If no MCU (CM4) firmware is running then no problems, but otherwise if I run MCU firmware (GPIO example) before shutting down MPU I get the following error after pushing...

alexey.b by Associate II
  • 2274 Views
  • 2 replies
  • 0 kudos

Resolved! failed boot via tftp

I tried booting via TFTP boot and got the following reply​BOOTP broadcast 1BOOTP broadcast 2BOOTP broadcast 3DHCP client bound to address 192.168.1.2 (766 ms)missing environment variable: pxeuuidmissing environment variable: bootfileRetrieving file: ...

Jzhua by Associate III
  • 3497 Views
  • 4 replies
  • 0 kudos

I am running LinuxPTP on the STM32MP157-C DK2 board. Is it possible to obtain a PTP PPS output on the ETH1_PPS_OUT (PG8 pin)?

If it is possible is there an example or at least some guidance on how to implement the PPS output? Coming from Cortex-M4/RTOS development I am doing my best to learn Application Processor/Embedded Linux development.​

Secure SPI on STM32MP157-DK1

Hey everyone,I am working on STM32MP157-DK1 with trustzone cortex-A.I want to use SPI in secure side, but it's possible only with SPI6 that is not mapped to the outside.It's possible to activate SPI (1 ... 5) peripherals in secure side ? if not, why ...

simoBen47 by Associate III
  • 3054 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.