2019-11-05 6:03 AM
Hello,
I am working with stm32mp157c-dk2
I have read the GPIO related parts in documents and wiki. I have also used GPIO from M4 side.
Are the following statements correct ?
Discovery board STM32MP157C-DK2 has two types of GPIOs connector:
There are two ways to use them;
this is what I have understand from the documents. Did I understand correctly ?
Is something false or missing in the statements ?
2019-11-05 6:29 PM
Things to add:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.