2026-05-01 4:37 AM
Hi,
I have a OTP provisioning script that wrote OTP 1 with value 0x000000ff, executing a partial close of security state B. The board now passes ROM/FSBL/OP-TEE/U-Boot but resets when the Linux kernel probes the first RIF-protected peripheral (HPDMA3). Disabling HPDMA3 in DT causes the same reset on HPDMA2, indicating closed-state RIF policy is being enforced globally regardless of the device tree configuration applied by OP-TEE
Can the board be returned to a open state using an rma procedure?
Kind Regards,
Jack Redpath
2026-05-05 3:14 AM
Hi
Do you have the JTAG 5pins available? if so, you may try opening the BSEC using the procedure described in the RM457 life cycle management.
Can you tell more about this script that wrote OTP1 to 0xff? where does it come from?
Kind Regards
Olivier
2026-05-05 4:31 AM
OTP 1 was a red herring, we have an internal script that writes OTPs as part of our provisioning sequence. I have tested just writing OTP 246 which should set the build id and it runs into the same problem which I thought was strange. Doesn't seem to be related to anything security or RIF related:
I do have the JTAG available, could you point me to the RM457 life cycle management?
Kind Regards,
Jack Redpath
2026-05-05 4:35 AM
Also, we are using an Android image which is based on OpenSTDroid Starter package (Android 13, kernel 6.1, ST-v6.x bootloader stack), with customer-specific kernel DT and userspace on top. Secure-world (TF-A / OP-TEE) are unmodified from the OpenSTDroid Release
Kind Regards,
Jack Redpath
2026-05-05 4:57 AM
Hi @Jredpath
I was refering to the product Reference Manual RM0457
There is a described procedure to open the BSEC p308. By default the BSEC opening password is 0x0 (if not already programmed).
Kind Regards
Olivier
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.