2025-06-17 10:56 PM
Will the Linux driver for stm32mp257 automatically set the MAC address based on the chip UID?
Or do users need to set it themselves?
Why is the MAC address printed using dmesg different from the hardware address obtained from the command?
Thank you, looking forward to your reply~
2025-06-19 7:21 AM
Hi @bugman ,
Can you specify if you are on ST or Custom board ?
Thanks
Olivier
2025-06-19 10:25 PM
I am using Myir STM32MP257 board
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.