2022-06-07 12:59 AM
CPU: STM32mp153CAC
Problem:
CPU is unable to boot further because of error:
"ERROR: Node system_off_soc_mode not found"
I have temporarily commented out the panic in the TF-A
This allows us to boot further into u-boot and then linux. But I'm worried that this is creating problems down the line.
We do not use STPMIC1 chip, can this be the reason for this error?
I suspect that something is missing in the device-tree. I have attached it.
2022-06-07 12:59 AM
/* SPDX-License-Identifier: (GPL-2.0+ OR BSD-3-Clause) */
/*
* Copyright (C) STMicroelectronics 2022 - All Rights Reserved
* Author: STM32CubeMX code generation for STMicroelectronics.
*/
/* For more information on Device Tree configuration, please refer to
* https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
*/
/dts-v1/;
#include <dt-bindings/pinctrl/stm32-pinfunc.h>
#include <dt-bindings/clock/stm32mp1-clksrc.h>
#include <dt-bindings/soc/st,stm32-etzpc.h>
#include "stm32mp15-mx.dtsi"
#include "stm32mp153.dtsi"
#include "stm32mp15xc.dtsi"
#include "stm32mp15xxac-pinctrl.dtsi"
#include "stm32mp15-ddr.dtsi"
/* USER CODE BEGIN includes */
/* USER CODE END includes */
/ {
model = "Swarco custom board - openstlinux-5.10-dunfell-mp1-21-11-17";
compatible = "st,stm32mp153c-itc3_cpu_a7_rev5-mx", "st,stm32mp153";
memory@c0000000 {
device_type = "memory";
reg = <0xc0000000 0x20000000>;
/* USER CODE BEGIN memory */
/* USER CODE END memory */
};
/* USER CODE BEGIN root */
/* USER CODE END root */
clocks {
/* USER CODE BEGIN clocks */
/* USER CODE END clocks */
clk_lse: clk-lse {
/* USER CODE BEGIN clk_lse */
/* USER CODE END clk_lse */
};
clk_hse: clk-hse {
/* USER CODE BEGIN clk_hse */
/* USER CODE END clk_hse */
};
};
chosen {
stdout-path = "serial0:115200n8";
};
aliases {
serial0 = &uart4;
};
}; /*root*/
&pinctrl {
fmc_pins_mx: fmc_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('D', 0, AF12)>, /* FMC_D2 */
<STM32_PINMUX('D', 1, AF12)>, /* FMC_D3 */
<STM32_PINMUX('D', 4, AF12)>, /* FMC_NOE */
<STM32_PINMUX('D', 5, AF12)>, /* FMC_NWE */
<STM32_PINMUX('D', 11, AF12)>, /* FMC_CLE */
<STM32_PINMUX('D', 12, AF12)>, /* FMC_ALE */
<STM32_PINMUX('D', 14, AF12)>, /* FMC_D0 */
<STM32_PINMUX('D', 15, AF12)>, /* FMC_D1 */
<STM32_PINMUX('E', 7, AF12)>, /* FMC_D4 */
<STM32_PINMUX('E', 8, AF12)>, /* FMC_D5 */
<STM32_PINMUX('E', 9, AF12)>, /* FMC_D6 */
<STM32_PINMUX('E', 10, AF12)>, /* FMC_D7 */
<STM32_PINMUX('G', 9, AF12)>; /* FMC_NCE */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('D', 6, AF12)>; /* FMC_NWAIT */
bias-disable;
};
};
sdmmc1_pins_mx: sdmmc1_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('C', 8, AF12)>, /* SDMMC1_D0 */
<STM32_PINMUX('C', 9, AF12)>, /* SDMMC1_D1 */
<STM32_PINMUX('C', 10, AF12)>, /* SDMMC1_D2 */
<STM32_PINMUX('C', 11, AF12)>, /* SDMMC1_D3 */
<STM32_PINMUX('D', 2, AF12)>; /* SDMMC1_CMD */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('C', 12, AF12)>; /* SDMMC1_CK */
bias-disable;
drive-push-pull;
slew-rate = <3>;
};
};
uart4_pins_mx: uart4_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 11, AF6)>; /* UART4_RX */
bias-disable;
};
pins2 {
pinmux = <STM32_PINMUX('A', 12, AF6)>; /* UART4_TX */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
};
/* USER CODE BEGIN pinctrl */
/* USER CODE END pinctrl */
};
&pinctrl_z {
/* USER CODE BEGIN pinctrl_z */
/* USER CODE END pinctrl_z */
};
&bsec{
status = "okay";
secure-status = "okay";
/* USER CODE BEGIN bsec */
/* USER CODE END bsec */
};
&etzpc{
secure-status = "okay";
st,decprot = <
/*"NS_R S_W" peripherals*/
DECPROT(STM32MP1_ETZPC_DDRCTRL_ID, DECPROT_NS_R_S_W, DECPROT_LOCK)
DECPROT(STM32MP1_ETZPC_DDRPHYC_ID, DECPROT_NS_R_S_W, DECPROT_LOCK)
/*"Non Secured" peripherals*/
DECPROT(STM32MP1_ETZPC_ETH_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
DECPROT(STM32MP1_ETZPC_FMC_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
DECPROT(STM32MP1_ETZPC_I2C4_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
DECPROT(STM32MP1_ETZPC_DMA1_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
DECPROT(STM32MP1_ETZPC_DMAMUX_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
DECPROT(STM32MP1_ETZPC_FMC_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
DECPROT(STM32MP1_ETZPC_UART4_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
DECPROT(STM32MP1_ETZPC_UART5_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
DECPROT(STM32MP1_ETZPC_USART1_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
DECPROT(STM32MP1_ETZPC_USART2_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
DECPROT(STM32MP1_ETZPC_USART6_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
/*"Secured" peripherals*/
DECPROT(STM32MP1_ETZPC_STGENC_ID, DECPROT_S_RW, DECPROT_UNLOCK)
/*"Mcu Isolation" peripherals*/
DECPROT(STM32MP1_ETZPC_DMA2_ID, DECPROT_MCU_ISOLATION, DECPROT_UNLOCK)
/*Restriction: following IDs are not managed - please to use User-Section if needed:
STM32MP1_ETZPC_SRAMx_ID STM32MP1_ETZPC_RETRAM_ID STM32MP1_ETZPC_BKPSRAM_ID*/
/* USER CODE BEGIN etzpc_decprot */
/*STM32CubeMX generates a basic and standard configuration for ETZPC.
Additional device configurations can be added here if needed.
"etzpc" node could be also overloaded in "addons" User-Section.*/
/* USER CODE END etzpc_decprot */
>;
/* USER CODE BEGIN etzpc */
/* USER CODE END etzpc */
};
&fmc{
pinctrl-names = "default";
pinctrl-0 = <&fmc_pins_mx>;
status = "okay";
/* USER CODE BEGIN fmc */
/* USER CODE END fmc */
};
&rcc{
status = "okay";
secure-status = "okay";
st,csi-cal;
st,hsi-cal;
st,cal-sec = <60>;
st,clksrc = <
CLK_MPU_PLL1P
CLK_AXI_HSI
CLK_MCU_HSI
CLK_PLL12_HSI
CLK_PLL3_HSI
CLK_PLL4_HSI
CLK_RTC_LSI
CLK_MCO1_DISABLED
CLK_MCO2_DISABLED
>;
st,clkdiv = <
1 /*MPU*/
0 /*AXI*/
0 /*MCU*/
0 /*APB1*/
0 /*APB2*/
0 /*APB3*/
0 /*APB4*/
0 /*APB5*/
0 /*RTC*/
0 /*MCO1*/
0 /*MCO2*/
>;
st,pkcs = <
CLK_CKPER_DISABLED
CLK_FMC_ACLK
CLK_ETH_DISABLED
CLK_SDMMC12_HCLK6
CLK_STGEN_HSI
CLK_USBPHY_DISABLED
CLK_SPI2S1_DISABLED
CLK_SPI2S23_DISABLED
CLK_SPI45_DISABLED
CLK_SPI6_DISABLED
CLK_I2C46_DISABLED
CLK_SDMMC3_DISABLED
CLK_ADC_DISABLED
CLK_CEC_DISABLED
CLK_I2C12_DISABLED
CLK_I2C35_DISABLED
CLK_UART1_DISABLED
CLK_UART24_PCLK1
CLK_UART35_DISABLED
CLK_UART6_DISABLED
CLK_UART78_DISABLED
CLK_SPDIF_DISABLED
CLK_SAI1_DISABLED
CLK_SAI2_DISABLED
CLK_SAI3_DISABLED
CLK_SAI4_DISABLED
CLK_LPTIM1_DISABLED
CLK_LPTIM23_DISABLED
CLK_LPTIM45_DISABLED
>;
pll2:st,pll@1 {
compatible = "st,stm32mp1-pll";
reg = <1>;
cfg = < 3 24 1 1 1 PQR(0,0,1) >;
};
/* USER CODE BEGIN rcc */
/* USER CODE END rcc */
};
&rtc{
status = "okay";
secure-status = "okay";
/* USER CODE BEGIN rtc */
/* USER CODE END rtc */
};
&sdmmc1{
pinctrl-names = "default";
pinctrl-0 = <&sdmmc1_pins_mx>;
status = "okay";
/* USER CODE BEGIN sdmmc1 */
/* USER CODE END sdmmc1 */
};
&tamp{
status = "okay";
secure-status = "okay";
/* USER CODE BEGIN tamp */
/* USER CODE END tamp */
};
&uart4{
pinctrl-names = "default";
pinctrl-0 = <&uart4_pins_mx>;
status = "okay";
/* USER CODE BEGIN uart4 */
/* USER CODE END uart4 */
};
/* USER CODE BEGIN addons */
/* USER CODE END addons */
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.