2023-01-16 1:28 AM
Welcome,
why for STM32MP157FAA1 at "STM32MP1 Series DDR memory routing guidelines examples" there is no terminating resistors?
Solved! Go to Solution.
2023-01-18 3:11 AM
Hi @JBalc.1
The example STM32MP15XXAA_1DDR3Lx16 target DDR3L x16 where termination resistors are optional (single memory, addresses/commands are point to point, short wires).
Regards
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2023-01-17 9:10 AM
Hi JBalc.1 (Community Member)
Altium table length (provided in Altium projects) gives also the length to terminating resistor.
I hope this clarifies.
Rgds,
Olivier
2023-01-18 3:11 AM
Hi @JBalc.1
The example STM32MP15XXAA_1DDR3Lx16 target DDR3L x16 where termination resistors are optional (single memory, addresses/commands are point to point, short wires).
Regards
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.