STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TF-A v2.6-r1 kernel hang issue?

I have a custom build on the stm32mp157f dk2.stm TF-A v2.6-r1 or vanilla TF-A v2.7, using sp_min.stm U-boot 2020.10-r2 or vanilla Barebox-2022.06.I've also tried U-boot 2021.10-r1, but that one crashes the kernel even earlier.Kernel: vanilla 5.18/van...

Hi: I can't find qmake in 4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15. When I use qtcreater5.15, I can't create STM32 code.

When I use cmake,/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sysroots/x86_64-ostl_sdk-linux/usr/share/cmake-3.22/Modules/CMakeTestCXXCompiler.cmake:62: error: The C++ compiler "/opt/st/stm32mp1/4.0.1-openstlinux-5.15-yocto-k...

zxiao.4 by Associate III
  • 1628 Views
  • 1 replies
  • 0 kudos

Resolved! question about ecosystem4

Hi,I follow "https://wiki.st.com/stm32mpu/wiki/PMIC_hardware_components#Support_in_Cortex-A7_Secure" can port the ecosystem 3.0 on the kit "stm32mp157c-odyssey" successfully, but fail to port the ecosystem4.0.The error log is :" 14:13:55 : Start Embe...

zqizh.1 by Associate III
  • 3384 Views
  • 1 replies
  • 0 kudos

Stm32mp157a kernal booting issue

Hi,We are using stm32mp157a processor in my custom board.I have download stm32mp157a-dk1 discovery kit code.The difference between discovery board and my custom board is Debug Serial port Configuration.In Discovery Board The debug uart pins are PG11-...

Resolved! ENABLE_PARTITIONS_IMAGE not enabled

When I change the download directory for my yocto project in my local.conf file, this note pops up, what is this and should I do anything about it.NOTE: /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/meta-st/met...

Gencay by Associate III
  • 2798 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.