2023-11-01 5:15 AM
I have developed a custom stm32mp157c board with a nand IC as storage using the FMC peripheral. This has worked fine with kernel v5.15, but I am trying to upgrade to kernel v6.1 due to driver related issues of the ethernet switch. However I can't seem to detect the mtd device anymore with the new kernel. I have done some digging and it seems it might be related to the new sys bus driver for the etzpc. The nand driver (FMC2) does currently not seem to load at boot.
Can anyone point me in the right direction? Is dit an issue with my devicetree or is there something wrong in de kernel.
2023-11-27 2:43 AM
Hi ,
When changing to kernel 6.1 did you also upgrade BSP component accordingly ?
ST only validate kernel V6.1 on top of V5 ecosystem BSP components.
Olivier
2024-01-07 9:53 PM
Hi,
I'm having a similar issue migrating from ecosystem v3 to v5, even though running TFA, Optee, U-boot all running fine from the latest release.
I can see stm32-sys-bus enumerating all the peripherals, but the driver for memory-controller@58002000 (stm32mp1-fmc2-ebi) and subsequently nand-controller (stm32mp1-fmc2-nfc) never gets probed, so no rootfs...
Any ideas why this is happening?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.