2024-06-18 6:34 PM - edited 2024-06-20 3:13 PM
os: Ubuntu (wsl)
I am trying to follow the steps as below:
https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package#Installing_the_tools
However, step 6.2 Image flashing cannot be completed.
When I entered the command below, it iterated only for the tf-a-stm32mp157c-dk2-usb.stm32 file.
Here are printed messages.
root@jesong:/home/STM32MP157C-DK2/STM32MPU_workspace/STM32MP1-Ecosystem-v5.0.0/Starter-Package/stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/images/stm32mp1# STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp157c-dk2-optee.tsv
-------------------------------------------------------------------
STM32CubeProgrammer v2.16.0
-------------------------------------------------------------------
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 0049002E3338510939303435
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP15xx
Device type : MPU
Revision ID : --
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-dk2-usb.stm32
File : tf-a-stm32mp157c-dk2-usb.stm32
Size : 220.40 KB
Partition ID : 0x01
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:03.013
RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-dk2-usb.stm32
File : tf-a-stm32mp157c-dk2-usb.stm32
Size : 220.40 KB
Partition ID : 0x01
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:02.143
RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01
I've also attached part of my log.
2024-06-20 7:59 AM
HI @JE_SP
strange to have twice TF-A load in the log file (maybe just because you tried twice).
Could you share the console log (using ST-Link USB which should show a VCP on your PC) ?
I see "Ubuntu (wsl)" , do this mean you are running Linux on a Windows WSL machine ?
Could you try Cubeprogrammer on a Windows machine or a Linux native machine ?
Regards
2024-06-20 3:29 PM
Hi, @PatrickF
Thank you for your response.
I wrote to answer your question.
strange to have twice TF-A load in the log file (maybe just because you tried twice).
>> I think I wrote in a way that could lead to misunderstanding. (so I edited)
However, I entered that command only once.
Could you share the console log (using ST-Link USB which should show a VCP on your PC) ?
>> I already attached the log file, is there another way to get the log?
I got the log using "-log trace_optee.log" option.
Below is part of the contents of the file I attached.
07:50:12:005 -------------------------------------------------------------------
07:50:12:005 STM32CubeProgrammer v2.16.0
07:50:12:005 -------------------------------------------------------------------
07:50:12:005
07:50:12:005 Log output file: trace_optee.log
07:50:12:005 Command line: -c port=usb1 -w "flashlayout_st-image-weston/optee/FlashLayout_sdcard_stm32mp157c-dk2-optee.tsv" -log "trace_optee.log"
07:50:12:005
07:50:12:006
07:50:12:006
07:50:12:024 Device Descriptor:
07:50:12:024 |_bLength : 0x12
07:50:12:024 |_bDescriptorType : 0x01
07:50:12:024 |_bcdUSB : 0x0200
07:50:12:024 |_bDeviceClass : 0x00
07:50:12:024 |_bDeviceSubClass : 0x00
07:50:12:024 |_bDeviceProtocol : 0x00
07:50:12:024 |_bMaxPacketSize : 0x40
07:50:12:024 |_idVendor : 0x0483
07:50:12:024 |_idProduct : 0xdf11
07:50:12:024 |_bcdDevice : 0x0200
07:50:12:024 |_iManufacturer : 0x01
07:50:12:024 |_iProduct : 0x02
...
I see "Ubuntu (wsl)" , do this mean you are running Linux on a Windows WSL machine ?
>> Exactly Yes!!
Could you try Cubeprogrammer on a Windows machine or a Linux native machine ?
>> If my running in wsl could be causing the problem, I'll try again with the method you suggested.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.