2019-06-14 12:33 AM
Hello,
I have a STM32MP157C-DK2 board and did the hello world cross compile project with GTK and that work perfectly.
Now I am trying to do cross compiling with Qt Creator. I used the same compiler as the GTK project but Qt Creator give me an error: The compiler (arm-linux-generic-elf-32bit) cannot produce code for the Qt version (x86-linux-generic-elf-64bit).
Where I get a compatible qmake file for this compiler or how to generate it?
Regards Marius
2019-06-14 12:58 AM
2019-06-14 8:44 AM
You should have qmake inside your toolchain.
Perhaps you forgot to setup the cross compiler environment before calling it with QtCreator?
--
Marco Cavallini | KOAN sas | Bergamo - Italia
embedded software engineering
2019-06-17 2:25 AM
Thanks for your reply @koan .
There is no qmake file in the SDK.
I have no cross compiler environment because I only want to use QtCreator for developing.
Which Toolchain is for this board and include a qmake file?
2019-06-17 9:49 AM
Hi Marius,
as you may know, QtCreator is mainly inteded to be used for Qt development.
Setup QtCreator for GTK is very difficult and if you really med an IDE in this case I suggest to use Eclipse or Visual Studio Code.
--
Marco Cavallini | KOAN sas | Bergamo - Italia
embedded software engineering
2019-07-02 3:10 AM
After many attempts I managed to generate a qMake file with qt-everywhere 4.8. (worked with this tutorial)
There are no Qt librarys installed on the STM32MP157C-DK2 board. After running my compiled Hello World application I got an error saying that libqtgui4 is missing.
Then I started to build an image with Qt5 librarys. It took many hours but in the end it worked. (this tutorial )
I installed the image on my board and started the sample projects with Qt. It worked, the Qt5 librarys were installed. When I ran my Hello World project the same error occurred. I think it is because my Hello World application was built with Qt 4.8 and the image contains Qt 5.11 librarys.
So I have to create a Qt 5.11 project. In my virtual machine (Ubuntu 18.04) I installed qt-everywhere 5.11.2 and took the "gcc-linaro-7.4.1-2019.02-x86_64_arm-linux-gnueabihf" compiler. My configuration options are these here:
./configure -opensource -confirm-license -prefix /usr/local/Qt-5.11.2-arm -xplatform linux-arm-gnueabi-g++My qmake.conf looks like these:
#
# qmake configuration for building with arm-linux-gnueabi-g++
#
MAKEFILE_GENERATOR = UNIX
CONFIG += incremental
QMAKE_INCREMENTAL_STYLE = sublib
include(../common/linux.conf)
include(../common/gcc-base-unix.conf)
include(../common/g++-unix.conf)
# modifications to g++.conf
QMAKE_CC = /home/myuser/gcc-linaro-7.4.1-2019.02-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-gcc
QMAKE_CXX = /home/myuser/gcc-linaro-7.4.1-2019.02-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-g++
QMAKE_LINK = /home/myuser/gcc-linaro-7.4.1-2019.02-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-g++
QMAKE_LINK_SHLIB = /home/myuser/gcc-linaro-7.4.1-2019.02-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-g++
# modifications to linux.conf
QMAKE_AR = /home/myuser/gcc-linaro-7.4.1-2019.02-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-ar cqs
QMAKE_OBJCOPY = /home/myuser/gcc-linaro-7.4.1-2019.02-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-objcopy
QMAKE_NM = /home/myuser/gcc-linaro-7.4.1-2019.02-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-nm -P
QMAKE_STRIP = /home/myuser/gcc-linaro-7.4.1-2019.02-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-strip
load(qt_config)The paths to my compiler are correct, I already checked this.
I get the following error when running the upper ./configure command
Note: Also available for Linux: linux-clang linux-icc
Note: No wayland-egl support detected. Cross-toolkit compatibility disabled.
ERROR: The OpenGL functionality tests failed!
You might need to modify the include and library search paths by editing QMAKE_INCDIR_OPENGL[_ES2],
QMAKE_LIBDIR_OPENGL[_ES2] and QMAKE_LIBS_OPENGL[_ES2] in the mkspec for your platform.How can i fix this error?
I'm happy about every answer.
2019-07-04 7:06 AM
Hello @Marius
I suggest you to follow an easier way adopting our new configuration of the Yocto Project build system
See our recent post about it : http://www.koansoftware.com/en/content/yocto-project-meta-layer-stm32mp1-koan
Let me know if it works on your side too.
--
Marco Cavallini | KOAN sas | Bergamo - Italia
embedded software engineering
2019-08-11 7:35 PM
HI Koan,
thanks for the link but why is it broken now ?
2019-08-12 9:56 AM
@IYetk Thank you for pointing out the problem.
We just renewed our website and some links are missing.
Now I restored the missing link above and however it now redirects to the official page.
https://koansoftware.com/yocto-project-meta-layer-for-stm32mp1-by-koan/
I hope that this may be useful for you.
Best regards
--
Marco Cavallini | KOAN sas | Bergamo - Italia
embedded software engineering
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.