2023-02-06 10:12 AM
We recently udated from OpenSTLinux v2.1 to v4.1. The boot chain is solid, but occasionally we are getting TEE aborts (trace listed below). I am not sure exactly how to debug this, any help would be appreciated.
E/TC:1
E/TC:1 Core data-abort at address 0x2fff8805 (translation fault)
E/TC:1 fsr 0x00000207 ttbr0 0x2ffd8020 ttbr1 0x00000000 cidr 0x0
E/TC:1 cpu #1 cpsr 0x000001f3
E/TC:1 r0 0x2fff8805 r4 0x2ffda889 r8 0x2ffda889 r12 0xffffffe0
E/TC:1 r1 0x2ffcda91 r5 0x000000f7 r9 0x00000000 sp 0x2ffda788
E/TC:1 r2 0x2fff8805 r6 0x00000000 r10 0x2fff8805 lr 0x2ffcb297
E/TC:1 r3 0x2fff8806 r7 0x2ffda870 r11 0xffffffff pc 0x2ffcac80
E/TC:1 TEE load address @ 0x2ffc0000
E/TC:1 Panic 'abort outside thread context' at ?:0
Solved! Go to Solution.
2023-05-01 12:50 PM
Just in case anyone is interested, our problem was a simple device tree oversight. We had neglected to inlude the reserved memory for optee in our kernel device tree when updating from TF-A boot chain to OP-TEE boot chain:
```
optee@de000000 {
reg = <0xde000000 0x2000000>;
no-map;
};
```
2023-02-06 10:14 AM
Hello @Community member ,
please can you share the complete boot log?
Best Regards,
Kevin
2023-02-06 10:50 AM
Thanks, Kevin, for responding!
Some more context: we are building our own distribution using buildroot. On top of that we are running Nerves (Erlang BEAM / Elixir main application). The exception reliable presents when we do a firmware update through our web interface (Phoenix/Cowboy server). The firmware file uploads successfully (written to a read/write partition formatted as F2FS), and aborts when attempting to overwrite the GPT partition table. The partition table overwrite is how Nerves manages firmware A/B with fallback.
Attached is the boot log up to and including the abort.
2023-05-01 12:50 PM
Just in case anyone is interested, our problem was a simple device tree oversight. We had neglected to inlude the reserved memory for optee in our kernel device tree when updating from TF-A boot chain to OP-TEE boot chain:
```
optee@de000000 {
reg = <0xde000000 0x2000000>;
no-map;
};
```
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.