2023-04-30 1:20 PM
I'm using a custom stm32mp157a board with a DSI display.
If I enable uart8 using pins J8 (UART8_TX) and J9 (UART8_RX) the display driver (panel-sitronix-st7701.c) doesnt load properly and the display stays blank.
uart8 does work properly. If I disable uart8 the display works again.
2023-05-02 1:48 AM
Hello @Rc.1 ,
Please can you share your complete boot log and your dtb file used.
Does the problem occurs only in Linux or directly from the boot?
Best Regards,
Kevin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.