2021-11-10 10:30 PM
openstlinux-5.10-dunfell-mp1-21-07-21
I am building st-image-core image in a Ubuntu 20 container on Fedora 34.
Any ideas?
ERROR: u-boot-stm32mp-2020.10.r1-r0 do_packagedata: Can NOT get PRAUTO, exception No module named '_sysconfigdata'
NOTE: recipe u-boot-stm32mp-2020.10.r1-r0: task do_packagedata: Failed
ERROR: Logfile of failure stored in: /__w/meta-flutter/stm32mp15-dunfell/build-openstlinuxeglfs-stm32mp1-disco/tmp-glibc/work/stm32mp1_disco-ostl-linux-gnueabi/u-boot-stm32mp/2020.10.r1-r0/temp/log.do_packagedata.1303648
ERROR: Task (/__w/meta-flutter/stm32mp15-dunfell/layers/meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp_2020.10.bb:do_packagedata) failed with exit code '1'Searching the line 1 string indicates it may be related to a host contamination issue.
I'm trying to get a CI validation job running for my meta-flutter layer.
CI job: https://github.com/meta-flutter/meta-flutter/blob/jw/stm32mp15/.github/workflows/stm32mp15.yml
2021-11-18 8:57 AM
Adding INHERIT_remove = "uninative" gets it further with same failure:
ERROR: libxkbcommon-0.10.0-r0 do_packagedata: Can NOT get PRAUTO, exception No module named '_sysconfigdata'
ERROR: Logfile of failure stored in: /__w/meta-flutter/stm32mp15-dunfell/build-openstlinuxeglfs-stm32mp1-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/libxkbcommon/0.10.0-r0/temp/log.do_packagedata.82728
NOTE: recipe libxkbcommon-0.10.0-r0: task do_packagedata: FailedI don't hit this problem with straight poky, or other images. Something specific to the STM3215MP Yocto support.
Still an open issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.