IPCC between cortex M4 and cortex A7 in stm32mp157A
Hi,I want to communicate data between two cores i.e,cortex A7and cortex M4.Can anyone share IPCC example code for Both M4 and A7 in stm32mp157A
Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
Hi,I want to communicate data between two cores i.e,cortex A7and cortex M4.Can anyone share IPCC example code for Both M4 and A7 in stm32mp157A
Is there no driver support for VBAT and VSENSE monitoring via ADC on Linux for STM32MP157C?
Hello everyone I want to use external power for my STM32MP157A-DK1. I connect 5 volts directly to the Raspberry Connector. But the U-boot in the console tells me that I should use USB Type C. How do I change the U-boot so that I can use more than jus...
HelloA STM32MP15 deviceif flahs proccess is started with STMCube programmer, the proccess finished inmediatly saying "process sucessfull" so the device is not booting , in eMMC mode or SD mode
Hi All -I was attempting to build the Qt example images for the DK2, following the wiki directions here:https://wiki.st.com/stm32mpu/wiki/How_to_build_and_use_an_SDK_for_QTI got to the step where it's building the SDK, after compiling the image succe...
hi, I have been working on compiling an openstlinux image with yocto, when compiling the image with bitbake it does not show me any error, but when mounting the image on the SD card it shows me the error that it cannot find "uInitrd", check in the ...
Hi all,What is the most correct and easiest way to generate dtb for the STM32MP1?I tried following this : https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Developer_PackageLooks way complicated and I get below error :/opt/st/...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.