2021-11-22 8:17 AM
Hello,
I read the STM32MP boot process in this link.
And it is a generic Embedded Linux boot process (ROM, SPL, Uboot, Kernel).
But, when I read further about STM32MP I figured out that U-boot UEFI commands are enabled, and there is support for PXE network boot which is supported from UEFI environment which is in this case executed from U-boot. Also I found a GPT support on flash memories (eMMC, ..).
I'm asking is there a documentation about UEFI on STM32MP ? Like:
Thanks,
Talel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.