2020-10-26 3:35 AM
Hello everyone,
I received my STM32MP157C-DK2 device and I built a Buildroot-image and flashed it successfully.
I am new to STM32 and to the IoT field so perhaps you can orient me and tell me which Programs I need to do so. I want to write a "hello_world" program that sends hello_world every x-seconds to an Endpoint-rest through Wifi.
Is it possible to only use Linux Bash/Shell interface to execute my Program? (I am familiar to these) and like I said I am only testing some features here like the ability of the DK2 to interact with Endpoint-rests.
Thank you all and have a nice day.
2020-12-02 7:41 AM
2020-12-02 7:41 AM
2021-07-14 7:42 AM
Dear @Lukas Brückner,
thanks for the instructions!
When using 'brcmfmac43430-sdio.txt' as you suggested, you need to activate the 'Broadcom BRCM bcm43***' firmware at Target packages instead of 'Broadcom BRCM bcm43xx'. Otherwise 'brcm/brcmfmac43430-sdio.bin' will not be available on the target.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.