2021-07-09 6:48 AM
We are generated a code from the Cube MX and written the application its working fine in debug mode through JTAG. But we want to put it into the Sd card . For this what is the procedure and how to enable the cortex M4 controller form A7.
2021-07-09 6:51 AM
Hi @srikanth ,
You may found useful information related to M4 management in wiki, started from page :
https://wiki.st.com/stm32mpu/wiki/Coprocessor_management_overview
Hope it help
Olivier
2021-07-09 10:25 AM
Thank you for the reply . We loaded the .elf file generated from the cube ide to the address 0xC2000000. after loading from serial link . the cortex M4 code is not running . That is M4 code is not running . We are new to the linux .
2021-07-11 11:56 PM
Hi @srikanth ,
I recommend that you read few other wiki pages
https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2
https://wiki.st.com/stm32mpu/wiki/Boot_chain_overview
Regards.
2021-07-13 1:49 AM
Hi @srikanth
For your information, inside STM32CubeIDE Cortex-M4 project you have RemoteProc/ that contains fw_cortex_m4.sh script used to load .elf
It is copied onto STM32MPU typically under /usr/local/projects/<your_project>_CM4/
You should be able to load your .elf launching this script:
cd /usr/local/projects/<your_project>_CM4/
fw_cortex_m4.sh start
Then, you have to update Linux in order to launch this script at boot time.
Best Regards,
Ludovic
2021-07-13 9:49 PM
Thanks for the reply
1)Now i am able to start and run the M4 Processor through remote processor early boot.but i am unable to stop the M4 processor ,How can i do that?
2)How can i Allocate stack to Second A7 Processor in Uboot Level .
2021-07-15 3:00 AM
Hi @srikanth ,
You can stop the M4 processor using: ./fw_cortex_m4.sh stop
Not sure to get your second question, could you elaborate?
Best Regards;
LudovicR
2021-07-15 3:19 AM
we are initializing all the peripherals in core 0(first A7) after that we are triggering a core 1(Second A7) by using Tamp registers Core 1 needs some stack to run the code . But I have a doubt i.e, how to allocate stack for for core 1.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.