2019-10-04 12:43 PM
Hello,
I am applying the second scenario of example openamp_tty_echo_wakeup.
The scenario is to wake up and make the system run again from "MCU : running and MPU :Cstop".
My question: When MPU goes in Cstop mode with the command "echo mem > /sys/power/state", linux user space is suspended. Can linux do something in the background in this situation ? For example saving the messages in a file coming from M4 (ch0).
If not, do I need to bring MPU to Cstandby mode for this porpose ? I read the power modes in wiki,other docs and couldnt see any functional difference between MPU Cstop and MPU Cstandby.
Is there any command to bring the system from MCU : running and MPU :running" to "MCU : running and MPU :Cstandby" ?
(there is no example for this scenario)
tnx
2019-10-07 2:03 AM
Hi @IYetk
Doing "echo mem > /sys/power/state" put the whole linux and A7 in Low Power mode.
Whatever CStop or CStandby, linux is doing nothing in background.
Most of the time sending a message from M4 will be a wakeup source for A7.
>> Is there any command to bring the system from MCU : running and MPU :running" to "MCU : running and MPU :Cstandby" ?
The targeted low power mode is defined by the wake-up source.
It's the same command to enter the mode
Refer to AN5109
Note that we do NOT recommend this strategy. Wakeup A7 from CStandby request a MPU reset and complete Linux boot sequence.
This maybe long, and present many challenges to not impact the M4 running process.
Hope it help,
Olivier
2019-10-07 4:00 AM
thanks. it helped
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.