cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP153 freezes at suspend when DMA buffers are allocated with stm32_rpmsg_sdb

atessadri
Associate

Hi all,

   I work on a STM32MP153 device and I used the command echo mem > /sys/power/state to put CPU A7 in Cstop mode, but I still have MCU running.

Before to enter suspend mode I have shared some memory buffers with MCU M4 with virtio RPMSG (as recommended).

In such case the suspend procedure doesn't come to end and it freezes in the middle.

If DMA buffers are not allocated everything works.

I have stopped every write operation from MCU M4 to don't interfere with the suspend process, but it freezes as well.

 

Thank you in advance

   Andrea

1 ACCEPTED SOLUTION

Accepted Solutions
atessadri
Associate

With no_console_suspend I have been able to see that the suspend procedure is completed (so my assumption was wrong).

There is an issue in the coprocessor code preventing it to reach the point where it will wake-up Linux again.

So, it isn't related to DMA buffers allocation/deallocation.

 

  Andrea

View solution in original post

1 REPLY 1
atessadri
Associate

With no_console_suspend I have been able to see that the suspend procedure is completed (so my assumption was wrong).

There is an issue in the coprocessor code preventing it to reach the point where it will wake-up Linux again.

So, it isn't related to DMA buffers allocation/deallocation.

 

  Andrea

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.