2025-04-01 9:22 AM - edited 2025-04-06 7:08 AM
OPTEE builds fine on ECO 5.0 (just built it right now with ECO SDK 5.0).
OPTEE build fails on ECO 6.0 (SDK 6.0)
Both on the same machine.
Both using the same Cube-MX generated files and build commands used for both ECO versions.
LD build/core/all_objs.o
arm-ostl-linux-gnueabi-ld.bfd: cannot find libgcc.a: No such file or directory
Solved! Go to Solution.
2025-04-06 7:08 AM
I overlooked that the issue is actually mentioned in the OP-TEE wiki for the compiler option.
2025-04-06 7:08 AM
I overlooked that the issue is actually mentioned in the OP-TEE wiki for the compiler option.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.