2024-06-13 1:17 AM
drivers/firmware/arm_scmi/optee.c:202:32: error: ‘TEE_OCALL2_OUT_PARAM1_ERROR’ undeclared here (not in a function)
202 | PTA_SCMI_OCALL_ERROR = TEE_OCALL2_OUT_PARAM1_ERROR,
| ^~~~~~~~~~~~~~~~~~~~~~~~~~~
drivers/firmware/arm_scmi/optee.c:228:31: error: field ‘ocall_arg’ has incomplete type
228 | struct tee_ocall2_arg ocall_arg;
drivers/firmware/arm_scmi/optee.c: In function ‘setup_ocall_thread’:
drivers/firmware/arm_scmi/optee.c:518:38: error: ‘TEE_OCALL2_ARG_INIT’ undeclared (first use in this function)
518 | .ocall_arg = TEE_OCALL2_ARG_INIT,
I checked that the corresponding optee.c file does not declare the relevant variable.I'd really like to solve this problem. Thank you.
Solved! Go to Solution.
2024-06-14 12:13 AM
Thanks again for your reply. I have solved the problem.
I have reinstalled Ubuntu version 18.04 and it has compiled successfully.
thank you
Regards,
Shicheng Luo
2024-06-13 8:04 AM
Hi @Lsc2001 ,
I'd like to ask you a few questions to better understand your problem :
Regards,
Grégory
2024-06-13 6:41 PM
Thank you very much for your reply.I am learning MP135 development board.Let me explain my problem.
1.The Ubuntu version is 22.04
2.I followed the installation instructions to install the latest version of the Developer Package (SDK). Version 23.06.21.The kernel version is 6.1.28.
3.I follow exactly the steps in README to compile the kernel source.The previously mentioned problem occurred during compilation.
Thank you again for your reply and hope to hear from you again.
2024-06-14 12:08 AM
Hi,
You could check if your SDK is properly sourced when you are in the terminal where you start your build.
You can do a
$> echo $CC
and if you don't see anything, your SDK is not sourced and that is probably what is causing your error.
If not, could you share with me the commands you are using and the traces you are getting.
Regards,
Grégory
2024-06-14 12:13 AM
Thanks again for your reply. I have solved the problem.
I have reinstalled Ubuntu version 18.04 and it has compiled successfully.
thank you
Regards,
Shicheng Luo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.