STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to start M4 on startup of STM32MP1?

I realize this is probably a pretty basic question but I haven't found a way to have the M4 portion of the firmware startup when the STM32MP1 is powered up.  I'm currently using an STM32MP157D-DK1 board, if that helps. I was able to debug the code of...

JayDev by Senior II
  • 4904 Views
  • 3 replies
  • 0 kudos

VirtIO problem on STM32MP157C-DK2

Hi! I am working with stm32mp157c-dk2 and trying to establish communication between m4 and a7 cores. I analyze standard examples for this purpose, namely OpenAMP_TTY_echo. VIRT_UART initialization is presented here for m4 core:  log_info("Virtual UAR...

Ljubica by Associate II
  • 4603 Views
  • 5 replies
  • 0 kudos

Resolved! STM32MP157 input capture gives wrong value

Hello, I've tried measure period of  GPS PPS which is very high accuracy. I'm using TIM5 input capture mode, reset slave mode. The TIM5 CCR1 gives value 208877646 that is wrong because I use high accurate generator for sys clock. The right value is a...

alex_vm by Associate II
  • 2341 Views
  • 2 replies
  • 1 kudos

Resolved! vddcore voltage is unstable

Dears,I use STM32MP151FAD3 together with STPMIC1. Nowdays I monitored the voltage of vddcore and found it's not stable shown as below.Mostly it's around 1.2v while sometimes it's up to 1.33v .Referring to documentation, I guess it's casued by dynamic...

_cgi-bin_mmwebwx-bin_webwxgetmsgimg__&MsgID=7515540295550502950&skey=@crypt_dce42f5b_a52fee0d437397af06da53efe79478a2&mmweb_appid=wx_webfilehelper.jpeg

Power off without PMIC

Hi, we make custom board base on STM32MP15 and without PMIC and have problem with power off command.Does anyone know any document or hint about this? All research we have found always include PMIC.  

Dat Tran by Senior II
  • 5739 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.