2020-09-03 9:20 AM
Hi,
I want to make a bare-metal application (without Linux OS) on a STM32MP157C-DK2 Board.
I need to use the usb host controller from this board (that why I choose it: multiples USB socket) but in the projects created with CubeIde, I can only assign USBH_HS1 or USB_OTG_HS with the A7 runtime context and my application C code is under the folder project_CM4 wich seem related to only M4 context and not with A7 context
So, my question is simple: could we use a USB mass storage device with a bare-metal application on STM32MP157C-DK2 Board without a Linux distrib?
I am wondering because I can’t find either a HAL USB module as expected in the “stm32mp1xx_hal�? list as if the only appropriate way to manage usb was with an OS attached to cortec A7
Thanks in advance for any help
2022-03-10 9:29 AM
Yes, of course you may use my work.
I had to uncomment the `if` block above, because the MSC driver from the ST USB library does not align the TX buffers to cache rows.
2022-03-10 11:10 AM
In my edition of ST device classes added alignment for needed structures:
see USBALIGN_BEGIN / USBALIGN_END usage in existing classes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.