2021-12-01 12:24 AM
Hi,
I'm using a STM32MP157a with yocto dunfell with 5.4 kernel version, and I'm trying to enable the kernel splashscreen. On my board I'm using the RBG lcd interface, and when the system is UP my application in showing curretly. On kernel config I have enabled the flags:
LOGO
LOGO_LINUX_CLUT224
FRAMEBUFFER_CONSOLE
but no tux are showing at startup...
Where I'm wrong ?
Solved! Go to Solution.
2022-01-10 9:36 AM
Hi @MRall.1 ,
To enable the spashscreen when building from Yocto, you have to build these two recipes:
The file psplash-drm.bb adds the file psplash-drm-start.service to your filesystem.
Once you are on the board, you must have something like that (I am on OpenSTLinux 5.10 so some paths may be different):
root@stm32mp1:/# find -name "psplash*"
./etc/systemd/system/local-fs.target.wants/psplash-drm-start.service
./lib/systemd/system/psplash-drm-start.service
./usr/bin/psplash-drm
./usr/bin/psplash-drm-quit
./var/lib/dpkg/info/psplash-drm.list
./var/lib/dpkg/info/psplash-drm.md5sums
./var/lib/dpkg/info/psplash-drm.postinst
./var/lib/dpkg/info/psplash-drm.prermHope it helps,
Regards,
Kevin
2022-01-10 9:36 AM
Hi @MRall.1 ,
To enable the spashscreen when building from Yocto, you have to build these two recipes:
The file psplash-drm.bb adds the file psplash-drm-start.service to your filesystem.
Once you are on the board, you must have something like that (I am on OpenSTLinux 5.10 so some paths may be different):
root@stm32mp1:/# find -name "psplash*"
./etc/systemd/system/local-fs.target.wants/psplash-drm-start.service
./lib/systemd/system/psplash-drm-start.service
./usr/bin/psplash-drm
./usr/bin/psplash-drm-quit
./var/lib/dpkg/info/psplash-drm.list
./var/lib/dpkg/info/psplash-drm.md5sums
./var/lib/dpkg/info/psplash-drm.postinst
./var/lib/dpkg/info/psplash-drm.prermHope it helps,
Regards,
Kevin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.