2021-08-16 4:36 AM
2022-01-10 1:50 AM
Hi @VRoma.2 ,
the package usbmount doesn't exist in OpenSTLinux distribution. However, could you make a try with the package udev-extraconf please? This package exists in 2.0.
root@stm32mp1:~# apt-get install udev-extraconfI did a test with OpenSTLinux 3.1 and my USB key is auto-mounted under /run/media/sda1. This is the output I got :
root@stm32mp1:~# [ 400.824653] usb 2-1.4: new high-speed USB device number 6 using ehci-platform
[ 401.011458] usb-storage 2-1.4:1.0: USB Mass Storage device detected
[ 401.022701] scsi host0: usb-storage 2-1.4:1.0
[ 402.205025] scsi 0:0:0:0: Direct-Access Kingston DataTraveler 3.0 PMAP PQ: 0 ANSI: 6
[ 402.220259] sd 0:0:0:0: Attached scsi generic sg0 type 0
[ 403.318695] sd 0:0:0:0: [sda] 30310400 512-byte logical blocks: (15.5 GB/14.5 GiB)
[ 403.327412] sd 0:0:0:0: [sda] Write Protect is off
[ 403.333210] sd 0:0:0:0: [sda] No Caching mode page found
[ 403.337185] sd 0:0:0:0: [sda] Assuming drive cache: write through
[ 403.490008] sda: sda1
[ 403.499969] sd 0:0:0:0: [sda] Attached SCSI removable disk
root@stm32mp1:~# cd /run/media/sda1/
root@stm32mp1:/run/media/sda1# ls
2016-01-09-10-PARIS-Ci JM ST ebooks
2016-01-09-10-PARIS-final JM_Work System Volume Information photos
Generiques_TV Papiers deces_claudeWhen unplugging the usb key, the key is un-mounted:
root@stm32mp1:/run/media/sda1# cd
root@stm32mp1:~# umount /run/media/sda1
root@stm32mp1:~# [ 706.654509] usb 2-1.4: USB disconnect, device number 6
root@stm32mp1:~# ls /run/media/
root@stm32mp1:~#Best regards,
--JM
2021-08-16 7:42 AM
Hi NPal.2 (Community Member)
Have you tried already: sudo apt-get install usbmount
Regards,
Olivier
2021-08-17 10:46 PM
Thanks @OlivierK . Will try that.
2022-01-08 8:11 AM
Is there no usbmount package under 2.0 dunfell InRelease?
I cannot install it, due to not found error...
2022-01-10 1:50 AM
Hi @VRoma.2 ,
the package usbmount doesn't exist in OpenSTLinux distribution. However, could you make a try with the package udev-extraconf please? This package exists in 2.0.
root@stm32mp1:~# apt-get install udev-extraconfI did a test with OpenSTLinux 3.1 and my USB key is auto-mounted under /run/media/sda1. This is the output I got :
root@stm32mp1:~# [ 400.824653] usb 2-1.4: new high-speed USB device number 6 using ehci-platform
[ 401.011458] usb-storage 2-1.4:1.0: USB Mass Storage device detected
[ 401.022701] scsi host0: usb-storage 2-1.4:1.0
[ 402.205025] scsi 0:0:0:0: Direct-Access Kingston DataTraveler 3.0 PMAP PQ: 0 ANSI: 6
[ 402.220259] sd 0:0:0:0: Attached scsi generic sg0 type 0
[ 403.318695] sd 0:0:0:0: [sda] 30310400 512-byte logical blocks: (15.5 GB/14.5 GiB)
[ 403.327412] sd 0:0:0:0: [sda] Write Protect is off
[ 403.333210] sd 0:0:0:0: [sda] No Caching mode page found
[ 403.337185] sd 0:0:0:0: [sda] Assuming drive cache: write through
[ 403.490008] sda: sda1
[ 403.499969] sd 0:0:0:0: [sda] Attached SCSI removable disk
root@stm32mp1:~# cd /run/media/sda1/
root@stm32mp1:/run/media/sda1# ls
2016-01-09-10-PARIS-Ci JM ST ebooks
2016-01-09-10-PARIS-final JM_Work System Volume Information photos
Generiques_TV Papiers deces_claudeWhen unplugging the usb key, the key is un-mounted:
root@stm32mp1:/run/media/sda1# cd
root@stm32mp1:~# umount /run/media/sda1
root@stm32mp1:~# [ 706.654509] usb 2-1.4: USB disconnect, device number 6
root@stm32mp1:~# ls /run/media/
root@stm32mp1:~#Best regards,
--JM
2022-01-10 7:27 AM
Hi @Jean-Marc B (ST Employee)
Thank you very much, it worked!
2022-01-10 8:57 AM
Hello @VRoma.2
That's great! Thank you for your feedback!
I think @NPal.2 would be interested by this update too.
Best regards,
--JM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.