2021-01-27 8:00 PM
Hi:
When I do not enable sdmmc1 in the device tree , a null pointer error will appear, as follows:
Unable to handle kernel NULL pointer dereference at virtual address 00000020
[ 4.406546] pgd = b1eff48d
[ 4.409244] [00000020] *pgd=00000000
[ 4.412826] Internal error: Oops: 17 [#1] PREEMPT SMP ARM
[ 4.418223] Modules linked in:
[ 4.421278] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 5.4.31 #1
[ 4.426906] mmc0: new high speed SDIO card at address 0001
[ 4.427205] Hardware name: STM32 (Device Tree Support)
[ 4.437847] PC is at mp1_mgate_clk_disable_safe+0x38/0x8c
[ 4.443241] LR is at mp1_mgate_clk_disable_safe+0x10/0x8c
[ 4.448644] pc : [<c06304bc>] lr : [<c0630494>] psr: 60000093
[ 4.454918] sp : df083eb0 ip : 00000000 fp : 00000008
[ 4.460149] r10: 0000013a r9 : c11004a4 r8 : c115f858
[ 4.465380] r7 : 00000000 r6 : 00000000 r5 : d1854cc0 r4 : d1852cc0
[ 4.471919] r3 : 00000000 r2 : c131bb04 r1 : 00000001 r0 : d1852cc0
[ 4.478459] Flags: nZCv IRQs off FIQs on Mode SVC_32 ISA ARM Segment none
[ 4.485693] Control: 10c5387d Table: d1c3c06a DAC: 00000051
[ 4.491447] Process swapper/0 (pid: 1, stack limit = 0x078a7dc4)
[ 4.497460] Stack: (0xdf083eb0 to 0xdf084000)
[ 4.501823] 3ea0: 60000013 d1854cc0 c12c07a0 00000000
[ 4.510023] 3ec0: c115f858 c06280d0 d1854cc0 d1841240 ffffe000 00000000 c115f858 c0628018
[ 4.518216] 3ee0: d1841240 c131a950 ffffe000 00000000 c115f858 c062a148 c12bdaa0 c062a110
[ 4.526413] 3f00: ffffe000 c0102fa8 00000001 c0168738 c109a538 c1100400 c0f8dfb4 00000000
[ 4.534606] 3f20: 00000007 00000007 00000000 c0f11e78 c0f0309c c0f03050 c11731f0 dffffdff
[ 4.542801] 3f40: dffffe07 c1204e88 cccccccd 00000007 c12f18c0 c1204e88 c115f834 c1173e04
[ 4.550998] 3f60: c12f18c0 c12f18c0 c115f838 c1101110 00000007 00000007 00000000 c11004a4
[ 4.559191] 3f80: c0c022a8 00000000 c0c022a8 00000000 00000000 00000000 00000000 00000000
[ 4.567387] 3fa0: 00000000 c0c022b0 00000000 c01010e8 00000000 00000000 00000000 00000000
[ 4.575582] 3fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 4.583776] 3fe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000
[ 4.591993] [<c06304bc>] (mp1_mgate_clk_disable_safe) from [<c06280d0>] (clk_disable_unused_subtree+0xdc/0x260)
[ 4.602087] [<c06280d0>] (clk_disable_unused_subtree) from [<c0628018>] (clk_disable_unused_subtree+0x24/0x260)
[ 4.612200] [<c0628018>] (clk_disable_unused_subtree) from [<c062a148>] (clk_disable_unused+0x38/0x128)
[ 4.621617] [<c062a148>] (clk_disable_unused) from [<c0102fa8>] (do_one_initcall+0x58/0x2b4)
[ 4.630077] [<c0102fa8>] (do_one_initcall) from [<c1101110>] (kernel_init_freeable+0x1c8/0x264)
[ 4.638790] [<c1101110>] (kernel_init_freeable) from [<c0c022b0>] (kernel_init+0x8/0x110)
[ 4.646986] [<c0c022b0>] (kernel_init) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
[ 4.654558] Exception stack(0xdf083fb0 to 0xdf083ff8)
[ 4.659618] 3fa0: 00000000 00000000 00000000 00000000
[ 4.667818] 3fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 4.676008] 3fe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 4.682637] Code: e5933004 e3530000 18bd81f0 e590606c (e5963020)
[ 4.688736] ---[ end trace e4f79bf44d365709 ]---
[ 4.693361] note: swapper/0[1] exited with preempt_count 1
[ 4.698849] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[ 5.790685] SMP: failed to stop secondary CPUs
[ 5.793669] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b ]---
How can I fix this problem? kernel version is 5.4.31
Best regard!
2021-01-27 8:04 PM
sdmmc1 device tree configuration:
&sdmmc1 {
pinctrl-names = "default", "opendrain", "sleep";
pinctrl-0 = <&sdmmc1_b4_pins_a>;
pinctrl-1 = <&sdmmc1_b4_od_pins_a>;
pinctrl-2 = <&sdmmc1_b4_sleep_pins_a>;
broken-cd;
st,neg-edge;
bus-width = <4>;
vmmc-supply = <&vdd_sd>;
status = "disabled";
};
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.