STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How can I prevent the contents of "RETRAM" from being erased? (base on linux with m4 rproc)

Hi all.I want to prevent the contents of "RETRAM" from being erased when I run the firmware with m4 rproc on "OpenSTLinux"."RETRAM" is powered by the battery through the VBAT pin to maintain data.To this end, TF-A was also modified to set and maintai...

Machilus by Associate III
  • 2004 Views
  • 3 replies
  • 0 kudos

Resolved! No wlan0 on DK1 I just received.

I have a pair of DK1 boards I just received that I wanted to get working with wifi direct, but neither even can show a wlan0 interface. In the past I have used a DK2 with buildroot and got the wlan0, and a coworker used stock yocto build on the DK2 a...

BillR by Senior
  • 1442 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.