2021-01-27 7:45 AM
Hi,
for our testing i want to activate the fullspeed OTG on the Pins PA11,PA12. VBUS_OTG is not routet out the Chip on the DK2.
Is it possbile to use the FS phy on PA11/PA12 on the DK2 board?
Best regards,
Niklas
2021-01-27 8:09 AM
Hi,
please look at https://wiki.st.com/stm32mpu/wiki/OTG_device_tree_configuration#DT_configuration_example_as_full-speed_OTG-2C_with_micro-B_connector
PA11 and PA12 are available on DK2, but not PA10 (ID) nor VBUS, so depending if you want OTG in host or device mode, you will have to add some DT keys to ignore the pins status.
See https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board#USB_OTG_node
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.