2024-07-15 8:04 AM - edited 2024-07-15 8:10 AM
I am creating a custom yocto image on a STM32MP157F-DK2. I am using the meta-stm32mp layer as apart of the bitbake build.
Yocto version : Scarthgap
When I run bitbake I get this failure
ERROR: hydra-image-1.0-r0 do_rootfs: Postinstall scriptlets of ['busybox'] have failed. If the intention is to defer them to first boot,
then please place them into pkg_postinst_ontarget:${PN} ().
Deferring to first boot via 'exit 1' is no longer supported.
Details of the failure are in /home/hydra/yocto/build/tmp/work/stm32mp1_brady-hydra-linux-gnueabi/hydra-image/1.0/temp/log.do_rootfs.
ERROR: Logfile of failure stored in: /home/hydra/yocto/build/tmp/work/stm32mp1_brady-hydra-linux-gnueabi/hydra-image/1.0/temp/log.do_rootfs.661419
ERROR: Task (/home/hydra/yocto/layers/poky/../meta-brady/recipes-core/images/hydra-image.bb:do_rootfs) failed with exit code '1'
Log file
update-alternatives: Linking /home/hydra/yocto/build/tmp/work/stm32mp1_brady-hydra-linux-gnueabi/hydra-image/1.0/rootfs/usr/sbin/sysctl to /usr/bin/busybox.nosuid
update-alternatives: Linking /home/hydra/yocto/build/tmp/work/stm32mp1_brady-hydra-linux-gnueabi/hydra-image/1.0/rootfs/usr/sbin/udhcpc to /usr/bin/busybox.nosuid
update-alternatives: Error: not linking /home/hydra/yocto/build/tmp/work/stm32mp1_brady-hydra-linux-gnueabi/hydra-image/1.0/rootfs/usr/sbin/watchdog to /usr/bin/busybox.nosuid since /home/hydra/yocto/build/tmp/work/stm32mp1_brady-hydra-linux-gnueabi/hydra-image/1.0/rootfs/usr/sbin/watchdog exists and is not a link
update-alternatives: Linking /home/hydra/yocto/build/tmp/work/stm32mp1_brady-hydra-linux-gnueabi/hydra-image/1.0/rootfs/usr/sbin/klogd to /usr/bin/busybox.nosuid
update-alternatives: Linking /home/hydra/yocto/build/tmp/work/stm32mp1_brady-hydra-linux-gnueabi/hydra-image/1.0/rootfs/usr/sbin/syslogd to /usr/bin/busybox.nosuid
I do not understand why I am getting this error. If I append the busybox recipe in my custom layer and set the CONFIG_WATCHDOG variable to 'n' then the image with build with no failure and boot on the board. I am assuming that some other layer is creating this .../user/sbin/watchdog directory, but I have been unsuccessful in finding that.
Any help would be appreciated, thanks.
2024-08-02 5:25 AM
Hi @nielsenni101 ,
Seems you are using Scarthgap wich is not yet supported by ST delivery. ( plan in next DV6 by end of year)
For time being we recommend to stick on Mickledore DV5.1 delivery.
Olivier
2025-11-10 12:04 PM
This is still occurring with Scarthgap.
I'm using the st-image-core, only modified with ' INIT_MANAGER = "sysvinit" '.
The devicetrees do have the watchdog configured though and I think the sbin comes from that.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.