2022-01-21 11:12 AM
“Error: failed to download Segment[0]�?
I looked at the other items with the same title but did not see an answer that would help me.
I am using the STM32MP157F-DK2
The demo code was working when box was opened
I tried to run the demo
“Populate the target and boot the image�?
at
https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2
I am using ecosystem release v3.1.0
And
STM32CubeProgrammer 2.9.0
Down load eventually fails with “Error: failed to download Segment[0]�?
Any help on the matter would be appreciated
Below is the Log
10:53:37 : USB speed : High Speed (480MBit/s)
10:53:37 : Manuf. ID : STMicroelectronics
10:53:37 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
10:53:37 : SN : 002A001B3438511436383238
10:53:37 : FW version : 0x0110
10:53:37 : Board : --
10:53:37 : Device ID : 0x0500
10:53:48 : Start Embedded Flashing service
10:53:48 : Memory Programming ...
10:53:48 : Opening and parsing file: tf-a-stm32mp157f-dk2-usb.stm32
10:53:48 : File : tf-a-stm32mp157f-dk2-usb.stm32
10:53:48 : Size : 225596 Bytes
10:53:48 : Partition ID : 0x01
10:53:48 : Download in Progress:
10:53:48 : File download complete
10:53:48 : Time elapsed during download operation: 00:00:00.473
10:53:48 : RUNNING Program ...
10:53:48 : PartID: :0x01
10:53:48 : Start operation done successfully at partition 0x01
10:53:48 : Flashlayout Programming ...
10:53:48 : Running Flashlayout Partition ...
10:53:48 : Flashlayout partition started successfully
10:53:48 : Memory Programming ...
10:53:48 : Opening and parsing file: fip-stm32mp157f-dk2-trusted.bin
10:53:48 : File : fip-stm32mp157f-dk2-trusted.bin
10:53:48 : Size : 1090807 Bytes
10:53:48 : Partition ID : 0x03
10:53:48 : Download in Progress:
10:53:50 : File download complete
10:53:50 : Time elapsed during download operation: 00:00:01.428
10:53:50 : RUNNING Program ...
10:53:50 : PartID: :0x03
10:53:50 : Reconnecting the device ...
10:53:53 : USB speed : High Speed (480MBit/s)
10:53:53 : Manuf. ID : STMicroelectronics
10:53:53 : Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
10:53:53 : SN : 002A001B3438511436383238
10:53:53 : FW version : 0x0110
10:53:53 : Board : --
10:53:53 : Device ID : 0x0500
10:53:53 : Device name : STM32MP157FAC Rev.Z
10:53:53 : Device type :
10:53:53 : Device CPU :
10:53:53 : Start operation done successfully at partition 0x03
10:53:53 : Memory Programming ...
10:53:53 : Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32
10:53:53 : File : tf-a-stm32mp157f-dk2-sdcard.stm32
10:53:53 : Size : 225489 Bytes
10:53:53 : Partition ID : 0x04
10:53:53 : Download in Progress:
10:53:56 : Error: failed to download Segment[0]
10:53:56 : Error: failed to download the File
10:53:56 : Error: Download partition 0x04 failed
10:53:56 : Error: TSV flashing service failed
10:53:56 : Warning: Connection to device 0x500 is lost
10:53:56 : Disconnected from device.
Solved! Go to Solution.
2022-02-01 12:53 PM
ran it again this time it failed the way it normally does
//////***************************************************************////
-------------------------------------------------------------------
STM32CubeProgrammer v2.9.0
-------------------------------------------------------------------
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 002A001B3438511436383238
FW version : 0x0110
Board : --
Device ID : 0x0500
AREA NAME SECT.NBR PARTITION.ID SIZE TYPE
Partition0 0000 0x00000000 0256 KB RW
FSBL 0000 0x00000001 0001 MB RW
Partition2 0000 0x00000002 0001 MB RW
Partition3 0000 0x00000003 0016 MB RW
Partition4 0000 0x00000004 0016 MB RW
virtual 0000 0x000000f1 0512 B R
Device name : STM32MP1
Device type : MPU
Revision ID : --
Device CPU : Cortex-A7
Start Embedded Flashing service
sending a set alternate setting request with index: 5
receiving packet
UpLoading data
sending a set alternate setting request with index: 1
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157f-dk2-usb.stm32
File : tf-a-stm32mp157f-dk2-usb.stm32
Size : 225596 Bytes
Partition ID : 0x01
Download in Progress:
Size : 225596 Bytes
Segment[0] downloaded successfully
File download complete
Time elapsed during download operation: 00:00:00.503
RUNNING Program ...
PartID: :0x01
sending a dfu end of download request
sending a set alternate setting request with index: 5
receiving packet
UpLoading data
sending a set alternate setting request with index: 0
Request detach value = 0
Start operation done successfully at partition 0x01
sending a set alternate setting request with index: 5
receiving packet
UpLoading data
sending a set alternate setting request with index: 0
Flashlayout Programming ...
Running Flashlayout Partition ...
sending a dfu end of download request
sending a set alternate setting request with index: 5
receiving packet
UpLoading data
sending a set alternate setting request with index: 3
Request detach value = 0
Flashlayout partition started successfully
sending a set alternate setting request with index: 5
receiving packet
UpLoading data
sending a set alternate setting request with index: 3
Memory Programming ...
Opening and parsing file: fip-stm32mp157f-dk2-trusted.bin
File : fip-stm32mp157f-dk2-trusted.bin
Size : 1090807 Bytes
Partition ID : 0x03
Download in Progress:
Size : 1090807 Bytes
Segment[0] downloaded successfully
File download complete
Time elapsed during download operation: 00:00:01.424
RUNNING Program ...
PartID: :0x03
sending a dfu end of download request
sending a set alternate setting request with index: 5
receiving packet
UpLoading data
sending a set alternate setting request with index: 0
Request detach value = 1
Reconnecting the device ...
Reconnecting...
Reconnected
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
SN : 002A001B3438511436383238
FW version : 0x0110
Board : --
Device ID : 0x0500
Device name : STM32MP157FAC Rev.Z
Device type : MPU
Device CPU : Cortex-A7
AREA NAME SECT.NBR PARTITION.ID SIZE TYPE
fsbl1 0000 0x00000004 0256 KB RW
fsbl2 0000 0x00000005 0256 KB RW
fip 0000 0x00000006 0004 MB RW
boot 0000 0x00000010 0064 MB RW
vendorfs 0000 0x00000011 0016 MB RW
rootfs 0000 0x00000012 0744 MB RW
userfs 0000 0x00000013 14364 MB RW
virtual 0000 0x000000f1 0512 B RW
OTP 0000 0x000000f2 1024 B RW
PMIC 0000 0x000000f4 0008 B RW
Start operation done successfully at partition 0x03
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 0
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32
File : tf-a-stm32mp157f-dk2-sdcard.stm32
Size : 225489 Bytes
Partition ID : 0x04
Download in Progress:
Size : 225489 Bytes
Segment[0] downloaded successfully
File download complete
Time elapsed during download operation: 00:00:00.072
RUNNING Program ...
PartID: :0x04
sending a dfu end of download request
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 1
Request detach value = 0
Start operation done successfully at partition 0x04
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 1
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32
File : tf-a-stm32mp157f-dk2-sdcard.stm32
Size : 225489 Bytes
Partition ID : 0x05
Download in Progress:
Size : 225489 Bytes
Error occured while downloading data
Status: errUNKNOWN, State: dfuERROR
Error: failed to download Segment[0]
Error: failed to download the File
Error: Download partition 0x05 failed
Error: TSV flashing service failed
2022-02-02 1:19 AM
Hi @JAmia.1 ,
Thank you for your log.
One more test, please can you try again the same command, but by replacing the file at the end of the command line with the file that I attached to my post.
The goal of this test is to flash during the two first steps, two files from 157c instead of 157f because 157c tf-a/fip are running at 650MHz.
Please send me the traces and tell me if it works.
Regards,
KEvin
2022-02-02 10:53 AM
ogrammer_CLI -c port=usb1 -vb 2 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157f-dk2-trusted_test_.tsv
-------------------------------------------------------------------
STM32CubeProgrammer v2.9.0
-------------------------------------------------------------------
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 002A001B3438511436383238
FW version : 0x0110
Board : --
Device ID : 0x0500
AREA NAME SECT.NBR PARTITION.ID SIZE TYPE
Partition0 0000 0x00000000 0256 KB RW
FSBL 0000 0x00000001 0001 MB RW
Partition2 0000 0x00000002 0001 MB RW
Partition3 0000 0x00000003 0016 MB RW
Partition4 0000 0x00000004 0016 MB RW
virtual 0000 0x000000f1 0512 B R
Device name : STM32MP1
Device type : MPU
Revision ID : --
Device CPU : Cortex-A7
Start Embedded Flashing service
sending a set alternate setting request with index: 5
receiving packet
UpLoading data
sending a set alternate setting request with index: 1
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-dk2-usb.stm32
File : tf-a-stm32mp157c-dk2-usb.stm32
Size : 225596 Bytes
Partition ID : 0x01
Download in Progress:
Size : 225596 Bytes
Segment[0] downloaded successfully
File download complete
Time elapsed during download operation: 00:00:00.568
RUNNING Program ...
PartID: :0x01
sending a dfu end of download request
sending a set alternate setting request with index: 5
receiving packet
UpLoading data
sending a set alternate setting request with index: 0
Request detach value = 0
Start operation done successfully at partition 0x01
sending a set alternate setting request with index: 5
receiving packet
UpLoading data
sending a set alternate setting request with index: 0
Flashlayout Programming ...
Running Flashlayout Partition ...
sending a dfu end of download request
sending a set alternate setting request with index: 5
receiving packet
UpLoading data
sending a set alternate setting request with index: 3
Request detach value = 0
Flashlayout partition started successfully
sending a set alternate setting request with index: 5
receiving packet
UpLoading data
sending a set alternate setting request with index: 3
Memory Programming ...
Opening and parsing file: fip-stm32mp157c-dk2-trusted.bin
File : fip-stm32mp157c-dk2-trusted.bin
Size : 1090377 Bytes
Partition ID : 0x03
Download in Progress:
Size : 1090377 Bytes
Segment[0] downloaded successfully
File download complete
Time elapsed during download operation: 00:00:01.464
RUNNING Program ...
PartID: :0x03
sending a dfu end of download request
sending a set alternate setting request with index: 5
receiving packet
UpLoading data
sending a set alternate setting request with index: 0
Request detach value = 1
Reconnecting the device ...
Reconnecting...
Reconnected
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
SN : 002A001B3438511436383238
FW version : 0x0110
Board : --
Device ID : 0x0500
Device name : STM32MP157FAC Rev.Z
Device type : MPU
Device CPU : Cortex-A7
AREA NAME SECT.NBR PARTITION.ID SIZE TYPE
fsbl1 0000 0x00000004 0256 KB RW
fsbl2 0000 0x00000005 0256 KB RW
fip 0000 0x00000006 0004 MB RW
boot 0000 0x00000010 0064 MB RW
vendorfs 0000 0x00000011 0016 MB RW
rootfs 0000 0x00000012 0744 MB RW
userfs 0000 0x00000013 14364 MB RW
virtual 0000 0x000000f1 0512 B RW
OTP 0000 0x000000f2 1024 B RW
PMIC 0000 0x000000f4 0008 B RW
Start operation done successfully at partition 0x03
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 0
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32
File : tf-a-stm32mp157f-dk2-sdcard.stm32
Size : 225489 Bytes
Partition ID : 0x04
Download in Progress:
Size : 225489 Bytes
Segment[0] downloaded successfully
File download complete
Time elapsed during download operation: 00:00:00.072
RUNNING Program ...
PartID: :0x04
sending a dfu end of download request
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 1
Request detach value = 0
Start operation done successfully at partition 0x04
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 1
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32
File : tf-a-stm32mp157f-dk2-sdcard.stm32
Size : 225489 Bytes
Partition ID : 0x05
Download in Progress:
Size : 225489 Bytes
Segment[0] downloaded successfully
File download complete
Time elapsed during download operation: 00:00:00.083
2022-02-02 10:55 AM
RUNNING Program ...
PartID: :0x05
sending a dfu end of download request
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 2
Request detach value = 0
Start operation done successfully at partition 0x05
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 2
Memory Programming ...
Opening and parsing file: fip-stm32mp157f-dk2-trusted.bin
File : fip-stm32mp157f-dk2-trusted.bin
Size : 1090807 Bytes
Partition ID : 0x06
Download in Progress:
Size : 1090807 Bytes
Segment[0] downloaded successfully
File download complete
Time elapsed during download operation: 00:00:00.391
RUNNING Program ...
PartID: :0x06
sending a dfu end of download request
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 3
Request detach value = 0
Start operation done successfully at partition 0x06
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 3
Memory Programming ...
Opening and parsing file: st-image-bootfs-openstlinux-weston-stm32mp1.ext4
File : st-image-bootfs-openstlinux-weston-stm32mp1.ext4
Size : 64 MBytes
Partition ID : 0x10
Download in Progress:
Size : 67108864 Bytes
Segment[0] downloaded successfully
File download complete
Time elapsed during download operation: 00:00:33.349
RUNNING Program ...
PartID: :0x10
sending a dfu end of download request
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 4
Request detach value = 0
Start operation done successfully at partition 0x10
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 4
Memory Programming ...
Opening and parsing file: st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
File : st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
Size : 16 MBytes
Partition ID : 0x11
Download in Progress:
Size : 16777216 Bytes
Segment[0] downloaded successfully
File download complete
Time elapsed during download operation: 00:00:08.599
RUNNING Program ...
PartID: :0x11
sending a dfu end of download request
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 5
Request detach value = 0
Start operation done successfully at partition 0x11
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 5
Memory Programming ...
Opening and parsing file: st-image-weston-openstlinux-weston-stm32mp1.ext4
File : st-image-weston-openstlinux-weston-stm32mp1.ext4
Size : 622752 KBytes
Partition ID : 0x12
Download in Progress:
Size : 104857600 Bytes
Segment[0] downloaded successfully
File download complete
Time elapsed during download operation: 00:05:29.957
RUNNING Program ...
PartID: :0x12
sending a dfu end of download request
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 6
Request detach value = 0
Start operation done successfully at partition 0x12
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
sending a set alternate setting request with index: 6
Memory Programming ...
Opening and parsing file: st-image-userfs-openstlinux-weston-stm32mp1.ext4
File : st-image-userfs-openstlinux-weston-stm32mp1.ext4
Size : 128 MBytes
Partition ID : 0x13
Download in Progress:
Size : 134217728 Bytes
Segment[0] downloaded successfully
File download complete
Time elapsed during download operation: 00:01:07.174
RUNNING Program ...
PartID: :0x13
sending a dfu end of download request
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
Request detach value = 0
Start operation done successfully at partition 0x13
sending a set alternate setting request with index: 7
receiving packet
UpLoading data
Flashing service completed successfully
2022-02-02 11:01 AM
That worked. had to enter log in two parts as it was to large.
Also note I changed the file name to _test_ as the command line did not like (test)
don't know if its worth repeating but
the file 157d-dk1- worked using the cube programmer
2022-02-03 2:04 AM
Hello @JAmia.1 ,
We identified an issue with 1 or 2 faulty boards, out of the box, with the same symptoms than yours, when running at 800MHz.
Unfortunately, you have to contact your supplier to have your board replaced.
Or you can continue to use it, but with 157c-dk2 files only.
Regards,
Kevin
2023-02-13 1:25 AM
I had the same issue in the STM32CubeProgrammer, but solved it somehow in another way:
In Erasing & Programming tab:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.