2024-09-05 4:31 AM - last edited on 2024-09-05 6:48 AM by mƎALLEm
hi please.
NOTICE: CPU: STM32MP157DAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157F-DK2 Discovery Board
INFO: PMIC version = 0x21
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: FCONF: Reading firmware configuration information for: stm32mp_fuse
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.8-stm32mp1-r2.0(debug):lts-v2.8.15-dirty(567af710)
NOTICE: BL2: Built : 00:51:33, Jan 26 2024
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
ERROR: DDR addr bus test: can't access memory @ 0xc0000004
PANIC at PC : 0x2ffebb4d
Exception mode=0x00000016 at: 0x2ffebb4d
even i did not change pin of the DDR with processor i used the same pin on custom board as it is like(stm32mp157f-dk2) board, and also the same RAM,
could you please help me out this or any thing we need to change
2024-09-05 4:56 AM
Even if you used the same pins as the reference board, differences in PCB layout (trace lengths, impedance, crosstalk, etc.) can affect signal integrity, leading to issues during DDR initialization.
2024-09-05 4:58 AM
so how i can manage this one where i need to modify , i am a fresher for this one please help me this project.
so where i need to modify the code , please
i am waiting for your response
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.