STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Teseo-Liv4F

Hello, We are evaluating the X-STM32MP-GNSS1 eval board on STM32MP-157F-DK2.The X-STM32MP-GNSS1 has Teseo-LIV3F GPS receiver on it, which does not support NAVIC.Since we want to test receiving signals from NAVIC specifically, can we replace the Teseo...

Quad SPI Transmit issue

 I'm working with the STM32MP131FAE in a bare-metal environment, and I'm experiencing issues with QuadSPI.I want to use Quad SPI to send 96 bytes of data continuously without any clock interruptions.However, currently, the data is being sent in chunk...

Stnoobs_0-1731320053002.png
Stnoobs by Associate II
  • 1162 Views
  • 0 replies
  • 0 kudos

Resolved! Linux image for a qt based app

Hi there STM team!I need to build a embedded Linux image for a STM32MP15 target. My application has a QT GUI already implemented. What is the best approach to create this image? I know OpenSTLinux exist but I don't fully understand what's the advanta...

JPabl.1 by Senior
  • 1645 Views
  • 1 replies
  • 1 kudos

build image

after following the bellow steps and in build-<distro>-<machine>/tmp-glibc/deploy/images/<machine> directoryi cant find the file system image(FlashLayout_sdcard_stm32mp157d-dk1-optee.tsv) in this directory as i am using stm32mp157d-dk1 and it contain...

Charan28 by Associate
  • 4489 Views
  • 1 replies
  • 0 kudos

Disabling TEE firmware

The following output seems to be the default: root@stm32mp2:~# cat /sys/class/remoteproc/remoteproc0/fw_format TEE  However, for debugging purposes, I would like to turn off firmware verification, and make the remoteproc driver accept plain ELF files...

manuelW by Associate
  • 1378 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.