2024-10-30 7:34 AM
Hi there ST team! I'm asking because I'm lost in all this process.
I have a QT quick app developer in QT Creator. I've already followed a tutorial from QT and I was able to flash the app in the STM32MP157F-dk2 using QT Creator.
Now, I want my target board to run an embedded Linux image, and the QT quick app to run in the user space of this distro.
I already installed the STM32MPU Starter package and can confirm the target runs the demo app as expected.
After this, I don't know how to continue. If I understand correctly, I need to:
1. install the STM32MPU developer package from https://wiki.st.com/stm32mpu/wiki/STM32MPU_Developer_Package#Checking_the_prerequisites
2. follow step 7.2 "Adding Linux user space application" from: https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package#Adding_a_.22hello_world.22_user_space_example
The problem is that step 7.2 mentions some folder that I don't know where it came from
cd <tag>/sources/<arm architecture>-<distro>-linux*Also, I understand this is just a simple "hello world" app, and I need to install QT related stuff.
The X-LINUX-QT expansion package seems to only work for stm32mp2 series, and I'm using STMMP1 series, so I think those tutorials won't work.
I'm following this tutorial: https://barenakedembedded.com/how-to-set-up-stm32mp1-with-qt/ but I'm getting a lot of errors so I'm not sure if that's the correct way to do it.
Any help in what to do after installing the starter package is sincerely appreciated :)
Solved! Go to Solution.
2024-11-09 6:57 AM
I can't access that page.
I wasn't able to build the yocto image that I needed by following the st tutorials, so I had to go the other way and start with a qt manifest.
I'm having some errors but at least that path seems more documented
2024-11-08 7:07 AM
Hi,
for MP1 started package and developer package support, you have to wait our next delivery that should come before end of 2024.
Current 1.0.0 X-LINUX-QT package only supports MP2. The meta layer can anyway be used for MP15. For MP135, it needs addition fixes (end of 2024 as well)
Sorry for the inconvenience.
Philippe.
2024-11-08 7:17 AM
You can also check this thread for MP1 setup:
https://stmicro.response.lithium.com/console/agent/22293782
2024-11-09 6:57 AM
I can't access that page.
I wasn't able to build the yocto image that I needed by following the st tutorials, so I had to go the other way and start with a qt manifest.
I'm having some errors but at least that path seems more documented
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.