STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP257F-DK USB C

I have a STM32MP257F-DK board and am using the OpenSTLinux image. I want to use the USB C connector on the board, but I noticed that the USB3DR internal peripheral page says that the peripheral can be assigned to the given runtime context, but it is ...

kgph99 by Associate
  • 1488 Views
  • 0 replies
  • 0 kudos

Bringing up STM32MP257 & Debug

We have built a SBC using the 257EV as a reference in Altium. We are trying to use debug. We have created a ST14 connector to connect to a STLink3 using UART 2 as the debug serial port.Is this possible, and should we use SWD or JTAG to debug the proc...

SCROGGYG by Associate II
  • 1648 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP135f VBat Current Consumption

Hello,We are trying to run Tamper block in VBat (Vsw) mode. When we powered off the device, Vbat pin consumes 3 - 5uA from the battery as specified in device user manual.As we understood from the documentation, the source of Vsw domain (either Vbat o...

GokhanK_0-1737966709048.png GokhanK_1-1737966792558.png GokhanK_2-1737968015962.png
GokhanK by Associate II
  • 5337 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.